Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

WaPi_297581
Level 2
Level 2
First like received

Hi all,

   

Working with a fresh install of Designer 5.4 SP1.

   

When attempting to build the following errors are thrown:

   

name translation failed on C:/Program\ Files\ (x86)/Cypress/PSOCDE~1/5.4/Common/CYPRES~1 - 3
name translation failed on C:\Program - 2
name translation failed on Files - 2
name translation failed on (x86)\Cypress\PSOCDE~1\5.4\Common\CYPRES~1\tools\include\CY8C22~2 - 3
make: *** No rule to make target `C:\PSoC', needed by `lib/obj/i2chwcommon.o'.  Stop.
 
B4347c1 - 1 error(s) 0 warning(s) 08:54:30

   

I attempted one 'fix' by following the directions at the bottom of the thread found here, but the error still persists after the reinstall.

   

This project was created on an 'old' workstation that has been replaced, the project was copied over to this new workstation without being modified in any way.

   

Any ideas?

2 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I would suggest to post in the PSoC1 forum. Which PSoC chip are you using?

   

 

   

Bob

0 Likes

This design uses the CY8C22345-24SXIT.

0 Likes