can i use same pin to drive led and pwm ??
i phasing problem with global selection.
STDCPU state is needed for led drive and GLOBALOUTPUT EVEN or ODD for pwm.
can i do with any register???
When a pin is connected to a signal a write to the data register will be overwritten by the signal.
Are you trying to connect an LED to a PWM? That will work. Just connect the LED to the PWM output pin.
Bob
No, i am using this pin in temperature controller for drive pwm or relay output.
can i use this pin alternatively as pwm and relay output??