Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

Hello, 

   

I am trying to sample 12 ADC channels and 8 I2C sensors at specific time periods. The timing is like this: 

   

A - 10ms - ADC 0, 1, 2

   

B - 50ms - I2C 0, 1, 2, 3

   

C - 100ms - ADC 3,4,5,6,7

   

D - 1000ms - ADC 8,9,10,11 and I2C 4,5,6,7

   

I am using a 12ch MUX, DelSig ADC, I2C bloc and for the specific timing generation multiple Frequency Dividers from the 1Khz ILO clock. 

   

The two ways I tried were: either read in each ISR all the relevant sensors  OR  set flags and execute in main using IFs ( if(ISR_flagSet -> read sensors)

   

Both are suboptimal solutions as the execution time varies, A is much faster than C and they don't work very well. An ideas are more than welcome. I need to read the sensors at fixed time to be able to integrate and differentiate them. 

   

I'm not sure this is possible using a single core MCU. 

0 Likes
6 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Use a fixed interrupt timing of 10ms = 100Hz and read all sensors, count the interrupts and and signal that an interrupt happened.

   

In the main-loop wait for the interrupt and act on the counter which result has to be considered in the current cycle

   

A - 10ms - ADC 0, 1, 2 each cycle

   

B - 50ms - I2C 0, 1, 2, 3 cycle %5 == 0

   

C - 100ms - ADC 3,4,5,6,7 cycle %10 == 0

   

D - 1000ms - ADC 8,9,10,11 and I2C 4,5,6,7 cycle %100 == 0 and reset cycle

   

When all sensor reading and calculations can be done within 10ms the time distances will be equal.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thanks Bob.  Reading the senors takes me different amounts of time: 
A = 4ms 
B = 115ms 
C = 8ms 
D = 140ms

I could probably optimize this a bit, maybe reduce the B and D to half but they are still very large. There isn't anything I can do, that's the amount I need for the sensor read (specific to the sensing element)
The idea is that I need to sample some sensors faster than others. 
What would you say is the best approach in this case? 

Thanks!

0 Likes
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted
        Problem is in I2C processing speed. How possibly operation B be repeated each 50 ms, while it takes 115ms to execute it? General approach should be: (i) since I2C in non-deterministic, no point to fight for timing accuracy; use buffers to collect incoming data, add some timestamp and process when system is idle. (ii) collect ADC data from all sensors on 10 ms interval into RAM using DMA, process when idle ( ignoring unnecessary data). Other thought: it takes ~100us to acquire 16 bit DelSigADC, why it takes about 1ms in your case? How many bits do you need?   
0 Likes
Anonymous
Not applicable

Hi. Thanks for the reply. It is my typo, B is only 11.5 not 115 😄 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Since you run interrupt driven you may trigger the I2C-readout 10ms before you need the values will reduce the wait-time for B to 1.5ms.

   

When D was a typo,too then wait-time will be 4ms.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

I wish it was... D is limited from the I2C sensor side to that time length. 

   

Regarding ADC sampling time - I use a moving average on the values and my code will need further improvements so it seems to add delay up. 

   

The way they were measured was using a toggle pin in the main loop before and after each batch of measurements.

   

 

   

So the best way would be to collect everything as fast as I can and just process it at desired times.

0 Likes