- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am trying to sample 12 ADC channels and 8 I2C sensors at specific time periods. The timing is like this:
A - 10ms - ADC 0, 1, 2
B - 50ms - I2C 0, 1, 2, 3
C - 100ms - ADC 3,4,5,6,7
D - 1000ms - ADC 8,9,10,11 and I2C 4,5,6,7
I am using a 12ch MUX, DelSig ADC, I2C bloc and for the specific timing generation multiple Frequency Dividers from the 1Khz ILO clock.
The two ways I tried were: either read in each ISR all the relevant sensors OR set flags and execute in main using IFs ( if(ISR_flagSet -> read sensors)
Both are suboptimal solutions as the execution time varies, A is much faster than C and they don't work very well. An ideas are more than welcome. I need to read the sensors at fixed time to be able to integrate and differentiate them.
I'm not sure this is possible using a single core MCU.
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Use a fixed interrupt timing of 10ms = 100Hz and read all sensors, count the interrupts and and signal that an interrupt happened.
In the main-loop wait for the interrupt and act on the counter which result has to be considered in the current cycle
A - 10ms - ADC 0, 1, 2 each cycle
B - 50ms - I2C 0, 1, 2, 3 cycle %5 == 0
C - 100ms - ADC 3,4,5,6,7 cycle %10 == 0
D - 1000ms - ADC 8,9,10,11 and I2C 4,5,6,7 cycle %100 == 0 and reset cycle
When all sensor reading and calculations can be done within 10ms the time distances will be equal.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks Bob. Reading the senors takes me different amounts of time:
A = 4ms
B = 115ms
C = 8ms
D = 140ms
I could probably optimize this a bit, maybe reduce the B and D to half but they are still very large. There isn't anything I can do, that's the amount I need for the sensor read (specific to the sensing element)
The idea is that I need to sample some sensors faster than others.
What would you say is the best approach in this case?
Thanks!
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
Hi. Thanks for the reply. It is my typo, B is only 11.5 not 115 😄
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Since you run interrupt driven you may trigger the I2C-readout 10ms before you need the values will reduce the wait-time for B to 1.5ms.
When D was a typo,too then wait-time will be 4ms.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I wish it was... D is limited from the I2C sensor side to that time length.
Regarding ADC sampling time - I use a moving average on the values and my code will need further improvements so it seems to add delay up.
The way they were measured was using a toggle pin in the main loop before and after each batch of measurements.
So the best way would be to collect everything as fast as I can and just process it at desired times.