Dear community,
I have a question about how exactly the emulated EEPROM function Write() works:
I have a constant array
const uint8 store[SIZEOF_EEPROM_ROW] = {};
Then I have an array
uint8 zustand[SIZEOF_EEPROM_ROW] = {};
zustand[0] = 3;
later in the code I use the Write function.
writeStatus = Em_Eeprom_Write(zustand,store,1);
I thought when the write function is done, the first entry of store array must be 3, but it is apperently not because when I test it:
if(store[0] == 3)
{
n++;
}
it just skips it.
Solved! Go to Solution.
I wonder whether the writeStatus is successful. Hence, please change it to, writeStatus = Em_EEPROM_Write(zustand[0], store, 1); the writeStatus will be successful. It writes one byte of data from source array (namely store in this case) to third logical position of Em_EEPROM data storage. If you read back the Em_EEPROM data storage, the third byte will be store[0]. Since store array is empty, please modify the firmware to following. For better understanding, please refer to Em_EEPROM datasheet.
const uint8 store[SIZEOF_EEPROM_ROW] = {11,22,33,44};
uint8 zustand[SIZEOF_EEPROM_ROW] = {};
zustand[0] = 3;
UART_PutString("EmEEPROM demo \n\r");
/*Initalize EEPROM with the start address of the memory location*/
eepromReturnValue = Em_EEPROM_Init((uint32_t)Em_EEPROM_em_EepromStorage);
/*Write contents to EEPROM */
eepromReturnValue = Em_EEPROM_Write(zustand[0], store, 1);
/*Read contents of EEPROM after write*/
eepromReturnValue = Em_EEPROM_Read(0, eepromArray, 10);
if(eepromArray[3]==11)
{
UART_PutString("The third position of Em_EEPROM storage is 11 \n\r");
}