Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

Hi,

   

We are currently in the process of verifying the components to be used in one of our projects and due to our experience with Cypress assistance and PSoC4 and PSoC5, we had decided to look into the option of using PSoC 5 for our new project.

   

The basic requirements for the project includes SPI, UART, I2C and CAN. the project also requires that the PSoC be connected to an external flash memory. The one we have taken into consideration is the Micron MT29F4G08ABADAWP-IT wherein the Data lines and the Address lines 8 bits in width and have the same pins. We had checked with PSoC Creator and saw the External Memory Interface component. We will be using the Asynchronous EMIF. However, the component has one line for the Address and one line for the Data.

   

Our choice for the external memory is not yet final and it can still be changed. What is the recommended external memory for PSoC5?

   

Thanks in Advance
K

0 Likes
1 Solution
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received
0 Likes
1 Reply
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

Hello,

   

You can look into this KBA for help regarding EMIF Component-

   

http://www.cypress.com/knowledge-base-article/external-memory-interface-support-psoc-3-psoc-5lp-kba8...

0 Likes