Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

I’m working on PSoC 5 kit. I want to sample my signal at a frequency of 360Hz with a resolution of 12bits. If I’m using delta-sigma ADC with a resolution of 12bits I can acquire a minimum of 4000 samples per second. Is there any alternative to reduce the number of samples?

0 Likes
3 Replies
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

  You can increase the resolution to 20 bits( and just take the first 12 bits) ,then you can get the frequency of 360 Hz from Delta -sigma ADC

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Another way is to use a timer with the desired frequency. Connect the timer to soc

   

or

   

Connect timer to an isr and read-out the ADC within the handler.

   

 

   

Bob

0 Likes
Anonymous
Not applicable
        Thank you for the responses.   
0 Likes