Hello everyone,
I'm developing a way to transfer data from the psoc to my pc and, so far I've managed to send 2048 16-bits values.
These values are obtained from an ADC that is directly connected to a DMA, so that I can save them in a buffer.
In order to save more values, I've read many entries, and the Application Notes as well, and I know I have to use TD chaining to obtain my desired result.
The thing is I have a small difference in comparison with the other entries. While they tend to have two or more buffers to save the ADC converted values, I only have one buffer (in my case, it is 16384 bytes long).
I tried to program each address for the TD's in the following manner:
TD[0] - 0...4095 -> destination address :0
TD[1] - 4096...8191 -> destination address :4096
TD[2] - 8192...12287 -> destination address :8192
TD[3] - 12288...16384 -> destination address :12288
My issue was that only the samples sent by the first TD resembled the wave originated from the ADC. Therefore, I'm asking you what could possibly be the mistake I made.
I'm not sure, but I think it's down to the TD properties, especifically, their destination addresses and some of the requests.
Thanks in advance
p.s my project is attached
Solved! Go to Solution.
Hello,
1)Is there any reason for enabling the CY_DMA_TD_AUTO_EXEC_NEXT option.
2)Can you enable TERM out for all TDs and check if the second TD and other TDs are getting executed.
3)Can you use '&' operator and check if you see any difference in behaviour?
CyDmaTdSetAddress(DMA_TD[0], LO16((uint32)ADC_DEC_SAMP_PTR), LO16((uint32)&samples.u16_buffer[0]));
CyDmaTdSetAddress(DMA_TD[1], LO16((uint32)ADC_DEC_SAMP_PTR), LO16((uint32)&samples.u16_buffer[4096]));
CyDmaTdSetAddress(DMA_TD[2], LO16((uint32)ADC_DEC_SAMP_PTR), LO16((uint32)&samples.u16_buffer[8192]));
CyDmaTdSetAddress(DMA_TD[3], LO16((uint32)ADC_DEC_SAMP_PTR), LO16((uint32)&samples.u16_buffer[12288]));
Thanks,
Hima
Hello,
1)Is there any reason for enabling the CY_DMA_TD_AUTO_EXEC_NEXT option.
2)Can you enable TERM out for all TDs and check if the second TD and other TDs are getting executed.
3)Can you use '&' operator and check if you see any difference in behaviour?
CyDmaTdSetAddress(DMA_TD[0], LO16((uint32)ADC_DEC_SAMP_PTR), LO16((uint32)&samples.u16_buffer[0]));
CyDmaTdSetAddress(DMA_TD[1], LO16((uint32)ADC_DEC_SAMP_PTR), LO16((uint32)&samples.u16_buffer[4096]));
CyDmaTdSetAddress(DMA_TD[2], LO16((uint32)ADC_DEC_SAMP_PTR), LO16((uint32)&samples.u16_buffer[8192]));
CyDmaTdSetAddress(DMA_TD[3], LO16((uint32)ADC_DEC_SAMP_PTR), LO16((uint32)&samples.u16_buffer[12288]));
Thanks,
Hima