Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

Hi,

   

 So i am doing a adc conversion via DMA which is triggered by a timer and Starts on an ISR which goes off on the start of the PWM Period.

   

My problem now is that sometimes my DMA interrupt works, then it doesnt as soon as i do something like insert a line which has nothing to do with the transfer like getting a timer value. Sometime when i set different Breakpoints it then startsto work again like it should but then again it bugs out as soon some minimum changes are made.

   

I have revised my code dozens of time but i´m not able to locate an error so i'm asking you guys.

   

Thank you in advance

   

Joe

   

*UPDATE* I am using the PSOC5 LP Prototyping Kit CY8CKIT-059

0 Likes
4 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Welcome to the forum, Joe!

   

You are a bit near at the edge of the chip performance with 1.25Msps of the ADC and 20000+ interrupts per second. I would suggest to control using a logic analyzer and some pins you trigger if your device programming is capable of that speed.

   

 

   

Bob

   

PS: Where in Germany are you located? I live near Bremen.

0 Likes
Anonymous
Not applicable

I'm in Baden-Würtemberg so thats far away plus this is kind of a study for my workplace(im a student) so direct help wouldn't be possible because i'm controlling classified electronics with the controller the code I provided is just some basic testing and calculation.
I already used a logic analyzer for displaying my adc results etc. but I need to be able to evaluate how long the programm needs for calculations and sampling for the study.
So if i got too much interrupts toning down sampling rate of the adc and the trigger-timing would help to be able to properly debug using the creator?

   

*UPDATE And just for Clarification my only interrupt which has issues is the DMA one ... all other interrupts trigger as they should and even reducing the interrupts to a minimum by just using continious mode and removing the adc_trigger ISR doesnt help either.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Can in the line

   

            adc_conversion[periodeAnz-j+i*periodeAnz] = (((2*adc_i_samples)-1024)*NdRI);

   

at j==0 and i == 50

   

a write outsides the array happen?

   

 

   

Bob

0 Likes
Anonymous
Not applicable

It shouldn't be possible to get into the loop at i=50 since at i=49 the loop increments i at the end of the for loop and then checks if the statement  i < sample_pro_periode  returns true which at i=50 is not the case so it exits the loop.

   

Greetings,

   

Joe

0 Likes