Announcements

Ever wondered how you could shape the future in collaboration with others? Join us at OktoberTech Asia Pacific and get inspired. Click here to sign up FREE of charge.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

madhu
Level 1
First reply posted First question asked Welcome!
Level 1

We have purchased the above IC from one of the open source as there were huge leadtime.

The IC snapshot is attached.

 

The IC part number/Body mark is CY8C3246AXI - 138 but in PsOC programmer it detects as CY8C3246AXI - 131. So we are unable to load the hex file of the program.

 

Can you help us?

0 Likes
1 Solution
Alakananda_BG
Moderator
Moderator 50 likes received 250 sign-ins 250 replies posted
Moderator

Hi @madhu ,

Infineon does not provide any assistance in the validation or testing of products not sourced from Infineon directly or one of Infineon’s authorized distributors.

Based from the below top marking, this is not valid Cypress/ IFX part.

Regards,

Alakananda

View solution in original post

0 Likes
4 Replies
Alakananda_BG
Moderator
Moderator 50 likes received 250 sign-ins 250 replies posted
Moderator

Hi,

Can you let us know from where you purchased the chip?

Can you also send the image of the chip.

Regards,

Alakananda
0 Likes
MaMi_1205306
Level 6
500 replies posted 50 solutions authored 25 likes received
Level 6

Hi,

 

As Alakananda-san said, by presenting an image of the company and device you purchased, you may be able to find out something from the lot number or date code.

 

As a way to use that part ...

The difference between CY8C3246AXI-131 and CY8C3246AXI-138 is the presence or absence of USB FS.

 

CY8C3246AXI-131 : not support USB FS

CY8C3246AXI-138 : support USB FS

 

If you are not using the USB FS component, you should be able to write by following the steps below:

1. Open project

2. Project menu => Device selector

3. Change CY8C3246AXI-138 to CY8C3246AXI-131

4. Rebuild

5. Write the HEX file of the corresponding folder with PSoC Programmer

 

I'm sorry but I can't understand the difference between the part number printed on the surface of the device and the part number recognized by the PSoC Programmer.

I think that the problem needs to be confirmed with the company that purchased it.

 

Regards,

0 Likes
madhu
Level 1
First reply posted First question asked Welcome!
Level 1

Dear Sir/Madam,

Thanks for below information.

Request your clarification on the below:

  1. Did you ever notice this kind of problem in the past?.
  2. How can be difference between the part number printed on the surface of the device and the part number recognized by the PSoC Programmer.
  3. Will it cause any adverse effect if we use this device after following below suggested correction in future?
  4. Can we use this device in our assembly or not?.

Thanks and regards,

MadhuPart purchased from Japan sourcePart purchased from Japan source

0 Likes
Alakananda_BG
Moderator
Moderator 50 likes received 250 sign-ins 250 replies posted
Moderator

Hi @madhu ,

Infineon does not provide any assistance in the validation or testing of products not sourced from Infineon directly or one of Infineon’s authorized distributors.

Based from the below top marking, this is not valid Cypress/ IFX part.

Regards,

Alakananda
0 Likes