Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

Hello,

I'm trying to do a DMA transfer of the capture value but I can not read anything.

image1.JPG

Configure of DMA :

#define DMA_BYTES_PER_BURST      4

#define DMA_REQUEST_PER_BURST    1

#define DMA_SRC_BASE              (CYDEV_PERIPH_BASE)

#define DMA_DST_BASE             (CYDEV_SRAM_BASE)

    Channel_Counter3 = DMA_Counter3_DmaInitialize(DMA_BYTES_PER_BURST, DMA_REQUEST_PER_BURST, HI16(DMA_SRC_BASE), HI16(DMA_DST_BASE));

    counter3_TD_0 = CyDmaTdAllocate();

    CyDmaTdSetConfiguration(counter3_TD_0, 4, counter3_TD_0, DMA_Counter3__TD_TERMOUT_EN | CY_DMA_TD_INC_SRC_ADR );

    CyDmaTdSetAddress(counter3_TD_0, LO16((uint32) Counter_3_STATICCOUNT_LSB_PTR), LO16((uint32)counter[2]));

    CyDmaChSetInitialTd(Channel_Counter3,counter3_TD_0);

    CyDmaChEnable(Channel_Counter3, (1u));

Captura.JPG

DMA hardware Request :Rising edge

Is something wrong?

I want to transfer the capture data and then active the interrupt and reset the counter.

Regards and thank you!

0 Likes
1 Solution
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

I don't see where the value of the counter is being transferred? Secondly, if you want to use interrupt, then why do you need a DMA? Some additional info about destination would help to answer your question.

View solution in original post

0 Likes
2 Replies
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

I don't see where the value of the counter is being transferred? Secondly, if you want to use interrupt, then why do you need a DMA? Some additional info about destination would help to answer your question.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

The enable input is fed with a very short pulse from the debouncer. Only while "enable" is high the counter will work.

Bob