Hello,
I'm trying to do a DMA transfer of the capture value but I can not read anything.
Configure of DMA :
#define DMA_BYTES_PER_BURST 4
#define DMA_REQUEST_PER_BURST 1
#define DMA_SRC_BASE (CYDEV_PERIPH_BASE)
#define DMA_DST_BASE (CYDEV_SRAM_BASE)
Channel_Counter3 = DMA_Counter3_DmaInitialize(DMA_BYTES_PER_BURST, DMA_REQUEST_PER_BURST, HI16(DMA_SRC_BASE), HI16(DMA_DST_BASE));
counter3_TD_0 = CyDmaTdAllocate();
CyDmaTdSetConfiguration(counter3_TD_0, 4, counter3_TD_0, DMA_Counter3__TD_TERMOUT_EN | CY_DMA_TD_INC_SRC_ADR );
CyDmaTdSetAddress(counter3_TD_0, LO16((uint32) Counter_3_STATICCOUNT_LSB_PTR), LO16((uint32)counter[2]));
CyDmaChSetInitialTd(Channel_Counter3,counter3_TD_0);
CyDmaChEnable(Channel_Counter3, (1u));
DMA hardware Request :Rising edge
Is something wrong?
I want to transfer the capture data and then active the interrupt and reset the counter.
Regards and thank you!
Solved! Go to Solution.
I don't see where the value of the counter is being transferred? Secondly, if you want to use interrupt, then why do you need a DMA? Some additional info about destination would help to answer your question.
I don't see where the value of the counter is being transferred? Secondly, if you want to use interrupt, then why do you need a DMA? Some additional info about destination would help to answer your question.
The enable input is fed with a very short pulse from the debouncer. Only while "enable" is high the counter will work.
Bob