- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am working with DHT11 temperature/humidity sensors and have one working like a charm. It uses a one-wire interface, so I need to both read and write the data pin. At the moment I have a function written that calls the pin name directly, but I'm trying to extend this to be able to handle four sensors. Since I have multiple reads/writes within the function I don't want to do an if/else or switch every time I need to access the pin. THe problem is that I don't know how to go about making the function generic so I can pass in the sensor number and have it work only with the correct pin. I looked at the aliases available for pin names, but I can't figure out how (or if it's even possible) to use a function parameter to indicate the correct alias to use with the CyPins_setpin(<alias>) function(s). I also looked at the Mux/Demux, but they are unidirectional so I don't think they'll work.
I don't feel like this post is very clear, but I'm having a difficult time coming up with better phrasing. I've attached a rough idea of what I'm trying to accomplish which will, hopefully, clarify things.
Any guidance on the correct way to approach this would be great.
Regards,
Matthew
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
This device has no address selection. The way I would do this is use a tri-state bus and have a selection control for the devices.
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
Maybe so?