Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
duno_297731
Level 3
Level 3
10 sign-ins 10 replies posted 10 questions asked

hello,

   

 

   

I have a control register (8 bit wide bus) in my schematic, and I want to take that bus and run it to two places.  the first destination is just a straight connection bit for bit.  for the other destination, I want to send the control register's upper 7 bits to the destinations lower 7 bits (a right shift, effectively) and concatenate a different wire onto the upper input.  

   

 

   

something like:
 

   

assign destination_reg[7:0] =  {single_bit , control_reg[7:1]}

   

 

   

such that if single_bit is 1, and control_reg was 00110101, that destination_reg[7:0] would be 10011010

   

 

   

what is the best way to do this in the schematic editor?  I don't know how to manipulate the buses well enough.  I could make 7 series-pairs of not gates (effectively a buffer), and assign the inputs to the upper bits of the control_reg bus, then assign the outputs to the lower bits of the destination_reg, but that's really messy.

0 Likes
3 Replies