Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 Hello,

   

This is my first time using PSoC Creator.  I'm also not an expert C guy, but getting up to speed.

   

The error resides in the device.h and is the only line of code:  #include <project.h>

   

I understand what device.h is, but can't find anything on project.h accept an Internet organization.

   

If this is just a general newbie C problem, could recommend some reading?

   

If not, please help with the specifics,

   

Thanks in advance.

0 Likes
3 Replies
Anonymous
Not applicable

Compile error: prj.M0121:can't open file 'project.h' (Newbie first time compile)

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

The project.h file is generated by the build process automatically.

   

 

   

Below is an example of an empty build on a PSOC 3 project.

   

 

   

Post your project archive, "file", "create workspace bundle" and forum can take a look at it.

   

 

   

Regards, Dana.

   

 

   

/*******************************************************************************
 * File Name: project.h
 * PSoC Creator 3.0 Component Pack 7
 *
 *  Description:
 *  This file is automatically generated by PSoC Creator and should not
 *  be edited by hand.
 *
 *
 ********************************************************************************
 * Copyright 2008-2013, Cypress Semiconductor Corporation.  All rights reserved.
 * You may use this file only in accordance with the license, terms, conditions,
 * disclaimers, and limitations in the end user license agreement accompanying
 * the software package with which this file was provided.
 ********************************************************************************/

#include <cyfitter_cfg.h>
#include <cydevice.h>
#include <cydevice_trm.h>
#include <cyfitter.h>
#include <cydisabledsheets.h>
#include <CyDmac.h>
#include <CyFlash.h>
#include <CyLib.h>
#include <cypins.h>
#include <cyPm.h>
#include <CySpc.h>
#include <cytypes.h>
#include <PSoC3_8051.h>

/*[]*/

Rachel
Level 1
Level 1
First reply posted First like given Welcome!

As a beginner, I also encountered this situation.
First build, project.h appears.
And then it compiles, and there are no errors.

0 Likes