Anonymous
Not applicable
Sep 07, 2016
11:53 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 07, 2016
11:53 AM
I'm trying to automate loading of firmware on a device via SWD. In order to do so, I'm running the CLI tool from a Windows CMD prompt. Everything starts fine but when I try to "Program" the device I get this error:
"Device is not in ISSP mode"
I try to set the device to program via SWD (SetProtocol 😎 but this does not seem to work. Is there some kind of trick I need to use to get this to work? The process works fine from the PSoC Programmer UI. When I try to script the process using the "runfile" command rather than typing into the CMD prompt I get the same error.
EDIT: This is with PSoC Programmer 3.24.4
Labels
- Labels:
-
PSoC 3
7 Replies