Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hi,

   

I'm new to Cypress controllers, I need to determine the most efficient controller for our application.

   

Our application specs:

   

-12 x  input (LVCMOS, LVTTL)

   

-1 CAN bus interface

   

-1 x output (PWM and/or DAC)

   

-1 x I2C interface

   

-SRAM interface (Density TBD) number of pins ? since Density is TBD (You can propose PNs with density under 2Mbits with package migration)

   

-embedded non volatile memory? Not critical, we can have it external.

   

 

   

What are the smallest packages (PN) that could handle most of the mentioned features?

   

 

   

The EAU is TBD. Lifetime is Critical.

   

 

   

Thank you in advance,

   

Pierre-Olivier Lessard

1 Solution
1 Reply