Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1

KJ_1509691
Level 1
Level 1

Hello,

Can I upgrade the KitProg firmware of my CY8CKIT-059 kit to KitProg3.

As I see that mode can be changed via the Programmer, so no need of switch and have to direct the additional IO's to the other headers.

I could find no information in this regards in the KitProg user guide.

The above kit is not listed in list of supported devices in the guide.

Thanks in advance.

Kuldeep

0 Likes
1 Solution
DheerajK_81
Moderator
Moderator First comment on KBA First comment on blog 5 questions asked
Moderator

Hello Kuldeep,

KitProg found on the CY8CKIT-059 kit cannot be upgraded to KitProg3 due to hardware limitations. The hardware design is unchanged between KitProg2 and KitProg3. As a result, any kit that supports KitProg2 can be upgraded to KitProg3.

As I see that mode can be changed via the Programmer, so no need of switch and have to direct the additional IO's to the other headers.

You can only change between the modes on KitProg by holding down the reset button of the kit for more than five seconds. There is no way to do this via any tool. Please refer to the KitProg User Guide for more information on this. However, with KitProg3, the mode switch is available to switch between the modes and also comes with a Firmware Loader CLI tool that you can use to switch between the modes. Since your kit does not support KitProg2, it is not listed as supported in the KitProg3 User Guide.

Regards,
Dheeraj

View solution in original post

1 Reply
DheerajK_81
Moderator
Moderator First comment on KBA First comment on blog 5 questions asked
Moderator

Hello Kuldeep,

KitProg found on the CY8CKIT-059 kit cannot be upgraded to KitProg3 due to hardware limitations. The hardware design is unchanged between KitProg2 and KitProg3. As a result, any kit that supports KitProg2 can be upgraded to KitProg3.

As I see that mode can be changed via the Programmer, so no need of switch and have to direct the additional IO's to the other headers.

You can only change between the modes on KitProg by holding down the reset button of the kit for more than five seconds. There is no way to do this via any tool. Please refer to the KitProg User Guide for more information on this. However, with KitProg3, the mode switch is available to switch between the modes and also comes with a Firmware Loader CLI tool that you can use to switch between the modes. Since your kit does not support KitProg2, it is not listed as supported in the KitProg3 User Guide.

Regards,
Dheeraj