Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

DaRe_2236336
Level 3
Level 3
First like given

I was wondering if this is possible since the motors I use do not have a tach signal?

1 Solution
JobinT_31
Employee
Employee
25 likes received 10 likes received 5 likes given

Hi David,

The Fan controller project provided with AN89346 http://www.cypress.com/file/137191/download

requires tach feedback and the project just provides PWM signal to control the motor. Not the actual BLDC motor drive signals.

Please check the input signal required to drive your Brushless DC motor.

If your motor requires direct BLDC signal you can refer: http://www.cypress.com/documentation/development-kitsboards/cy8ckit-037-psoc-4-motor-control-evaluat...    examples.

There are couple of projects available which doesn't need any external feedback.

# Sensorless BEMF based BLDC

# Sensorless FOC based.

Thanks

JobinGT

View solution in original post

0 Likes
1 Reply
JobinT_31
Employee
Employee
25 likes received 10 likes received 5 likes given

Hi David,

The Fan controller project provided with AN89346 http://www.cypress.com/file/137191/download

requires tach feedback and the project just provides PWM signal to control the motor. Not the actual BLDC motor drive signals.

Please check the input signal required to drive your Brushless DC motor.

If your motor requires direct BLDC signal you can refer: http://www.cypress.com/documentation/development-kitsboards/cy8ckit-037-psoc-4-motor-control-evaluat...    examples.

There are couple of projects available which doesn't need any external feedback.

# Sensorless BEMF based BLDC

# Sensorless FOC based.

Thanks

JobinGT

0 Likes