Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NaAm_1281831
Level 2
Level 2
First comment on KBA 10 replies posted 10 sign-ins

Hi,

I would like to use the USB port (not the THUMB Connector) on the Demo kit CY8CKIT-059,

and so I have taken working code example  "CE195277_ADC_and_UART01" and added the USBFS component (as per the directions of the codeexample USBFS_UART ) . It compiled good, but giving me error unrecognized USB device when I try to connect the USB port, I have tried to use the USBUART_CDC.inf file available under the code example directory, but I am getting the error saying it is not compatible with WINDOWS10 X64 platform,

Please let me know how to overcome this issue.

Please send me working project and USB driver file (.inf) in case to save the time back and forth.

Thanks,

Naga.

0 Likes
1 Solution
1 Reply
himam_31
Employee
Employee
50 likes received 25 likes received 10 likes received

Hello,

Can you have a look at this post:

CY8CKIT-50 PSOC5 development Kit USBUART driver not working on windows 10

Thanks,

Hima

0 Likes