Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

AbPa_4654881
Level 3
Level 3
10 replies posted 10 questions asked 10 likes given

Hi All, I  am working with cy8ckit-059, Suddenly when I tried to connect with the USB port of PC, the power led and status led blinks for a half second and the computer is not detecting it . Also the area near to F2 (FUSE on kit prog) is getting very HOT. I checked The continuity of FUSE it is not blown. and When I tried to connect cy8ckit-059 J6 port to microusb (while working with USBUART) The are near F1 (FUSE on psoc kit) is getting very HOT. As I have checked Both are fuse are not blown as It is showing continuous connection in multimeter. Is there any way I can fix this issue? I am not getting What Actually happened that causes this issue?

0 Likes
1 Reply
SrikanthD_56
Employee
Employee
First comment on blog 100 replies posted 50 solutions authored

Hi,

Sounds like your kit is drawing more than 500mA current or there is a short somewhere. Please remove any externally connected components, checks for any shorts and then try powering the kit again.

Cheers!

0 Likes