Hi guys!
I tried to program my PSoC5 today. Sadly, it is not recognized with the KitProg at all. I have 3.3V on all VDD pins and 1.8V on all VCC pins (generated from internal regulator. I have caps on every pin as explained in the application note. I also recieve a clock on the ck pin and data on the io pin of the SWD interface of the chip. So I am wondering: can I flash that thing with the CY8CKIT-042-BLE or is that my mistake? Or could it be that I broke the chip by applying 5V to the VCC pins (which I first mistakenly did ...)? Or is there something else I have to take into account?
Any help is very much appreciated.
Peace
Noah