Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi ,

I am working on this CY8C5267AXI-LP051 micro controller and I want to add  2MByte External flash,Kindly let me know how to use 2MB external flash on this micro controller.

Thanks ,

Raveen.

0 Likes
1 Solution
DheerajK_81
Moderator
Moderator
Moderator
First comment on KBA First comment on blog 5 questions asked

Hello Raveen,

PSoC Creator offers the External Memory Interface Component (EMIF) which can be used to interface with your 2Mb Flash.

These resources will be helpful:

1) http://www.cypress.com/documentation/code-examples/ce95312-external-memory-interface-emif-psoc-35lp 

2) Page#21: http://www.cypress.com/file/45916/download

3) http://www.cypress.com/file/135141/download

Regards,

Dheeraj

View solution in original post

0 Likes
5 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Depends on what interface you want to use. As long as you do not want to executer code from the flash memory you could use I2C or SPI interfaces. There is an external memory interface component, but I didn't check (yet) if that works with flash.

Just for curiosity: What do you need 2 MB for?

Bob

0 Likes
Anonymous
Not applicable

Thanks bob,

2MB flash for log data from device.I thought CY8C5267AXI-LP051 doesn't have SPI ,what about  UDBs and  I/O ports can I use that for external flash

pls refer this data sheet http://www.cypress.com/file/45916/download  at  5.6

0 Likes

There are plenty of interfaces on your chipbased on UDBs. They can be configured to act as UART, SPI, I2C and some more. I would suggest you to download and install Creator 4.2 and start a project with your selected device. The Component catalog will show what components are availlable and the resources tab will show (after a build) the usage.

Bob

0 Likes
Anonymous
Not applicable

Thanks bob

0 Likes
DheerajK_81
Moderator
Moderator
Moderator
First comment on KBA First comment on blog 5 questions asked

Hello Raveen,

PSoC Creator offers the External Memory Interface Component (EMIF) which can be used to interface with your 2Mb Flash.

These resources will be helpful:

1) http://www.cypress.com/documentation/code-examples/ce95312-external-memory-interface-emif-psoc-35lp 

2) Page#21: http://www.cypress.com/file/45916/download

3) http://www.cypress.com/file/135141/download

Regards,

Dheeraj

0 Likes