- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi everyone,
I try to read a 0 to 2.5V with the ADCINC14, i use the REFMUX for read 8 port, and I use the external ref (P2[4], P2[6]).
Analog Power : SC On/Ref High
Ref Mux : P2[4]+/-P2[6]
VDD : 5V
P2[4] : 0V
P2[6] : to a ref 2.5V
Problem; can't read more than ~15818 counts...
2^14 = 16384
ref 2.5V/16384 = 152.588uV
15818 * 152.588uV = 2.414V <- this is my problem, if the input is 2.5V or greater never read more than this.
Thanks for reading and helping me 🙂
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Corso,
I need to check this out but one thing which need to correct over here is the proper selection of ref voltage. With the current selection, negative voltage of the device is -2.5V because of P2[4] +/- P2[6]. You can connect a 1.25V signal on both the pins, this'll make the REFHI setting as 2.5V and REFLO as 0V.
I'll check this at my end and shall let you know.
Best regards,
Pushek