cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

Hi there, I'm new in this forum and new as a Miniprog3 user.
I just bought this programmer and I want to try it. I got a hex file example from here:
http://www.cypress.com/documentation/code-examples/ce54097-sleep-timer-user-module

   

and as soon as I try programming my CY7C64215 I receive an error message and the programming stops.
Apparently there is not enough memory on this device for the .hex file to be written, but I downloaded this example cause it was supposed to be suitable for my device.

I need an hex file to write (max 16k flash). Can someone help me? Any hex file suitable would be enough to start. Thank you

0 Likes
1 Solution
Bob_Marlowe
Expert II

At top of this page enter "CY7C64215" into the keywords field. Maybe you can find an example hex file.

   

 

   

Bob

View solution in original post

0 Likes
3 Replies
Bob_Marlowe
Expert II

The CY7C64215 is a USB controller, while the code example is for a PSoC1. This will not match at all.

   

What exactly do you want to perform? Learning PSoC? Then I would suggest you to get a CY8CKIT-059, a PSoC5 prototyping kit. See here.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thank you for your answer.
As I told I want to learn. But before that I want to test my Miniprog3, cause maybe it's not working. And when I'll be ready to understand it would be late to give back the programmer.
Now I have only CY7C64215 and I need to try with it.
I just need any hex file (doesn't matter much what the program does) that's suitable to program this  CY7C64215.
 

0 Likes
Bob_Marlowe
Expert II

At top of this page enter "CY7C64215" into the keywords field. Maybe you can find an example hex file.

   

 

   

Bob

0 Likes