When I enable differential mode on the PSoC 3 DelSigma ADC I get the following warning on buid:
Info: apr.M0002: Analog signal "\ADC_DelSig_1:Net_194\" is connected to one terminal only. (App=cydsfit)
I just have the ADC on the schematic with 2 analog pins feeding the input terminals. All the settings are at the default except the input range.
Is this warning safe to ignore or do I have larger problems?
This warning will not cause any issues with the functionality . This warning is because the component implementation generates a Vssa refernce while building , but is not using it.So it is connected to just one analog terminal. This will be corrected in the future versions of the component .
I still get the same warning. Versions :
PSoc Creator 3.0
Delta Sigma ADC [v3.0]
Is there a workaround ?