Bootloader Command not recognized

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
PaDa_2015331
Level 1
Level 1
First like received First like given

I have a product developped on PSOC3 and PSOC Creator 3.3.  For some reason, I wanted to migrate the design on PSOC Creator 4.2.  The design works well in 4.2 but when it cames to use Host Bootloader 4.2 to update the product I got the message "Command not recognized : the supported commands are defined in the Bootloader section of the System Refer Guide".  Even if I have this message, the upload seems to be succesful.

Also, If I use Host Bootloader 3.3 and I use the same .cyad file compiled from PSOC Creator 4.2, I don't get the message.

I know about the thread bootloader host - Command not recognised​  but it's not my case with the project name.

Any idea on what can cause it? Is the bootloader needs to be recompile in 4.2 or it should be the same as in 3.3?

Thanks.

0 Likes
1 Solution
GeonaP_26
Moderator
Moderator
Moderator
250 solutions authored 100 solutions authored 50 solutions authored

I am able to bootload a PSoC Creator 3.3 compiled bootloadable cyacd file using PSoC Creator 4.2 based Bootloader host. Could you share the working PSoC Creator 3.3 bootloader and bootlodable projects?

View solution in original post

0 Likes
1 Reply