- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The device is a CY8C29466-24PXI, PSoC 1, Designeer 4.4 .
I have this working with a CY8C27443-24PXI but I can not seem to get to work with this processor.
I want to write 64 bytes to 0x7f80, I have a ram buffer of 64 bytes called "rx_buffer" It also seems to take 2 or 3 seconds to come back from the write_eeprom code.
Ant help would be wonderful.
Thanks
Gord
- Labels:
-
PSoC 1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Welcome in the forum, Gord.
The processor of the Cy8C27xx and the Cy8C29xx are quite the same, only the 27443 has got 16K flash and only 256 bytes of sram. Hence there cannot be a large code difference.
The PSoC Designer is a bit outdated, I would suggest you to update to current version which is 5.4
Check if you set the Firstblock to 510.
Check if you modified the flash security to allow writes to the required blocks
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Bob
Firstblock is set to 510 and the flash security is set to U for the last 2 blocks but I cannot get it to write.
Would you have a assembly code snippet to share?
Thanks
Gord
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Only code snippets are in datasheet for eeprom. Check your stack and stack setting.
Switch over to PSoC4, more modern, cheaper, debug capabilities, but no DIL-package. Check the prototyping kit CY8CKIT-043.
Bob