Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1

Anonymous
Not applicable

I want to test a very simple code, insamp (with two PGA and one ADC). When I run the code, it stop in the line:

   

if (ADCINC_1_fIsDataAvailable() != 0);

   

Below is the code, can anyone tell me what wrongs, thankks a lot in advance!

   

#include <m8c.h>        // part specific constants and macros
#include "PSoCAPI.h"    // PSoC API definitions for all User Modules
#include "PSoCGPioInt.h"

   

int  iResult;

   

void main(void)
{
    PGA_1_Start(PGA_1_HIGHPOWER);
    PGA_2_Start(PGA_1_HIGHPOWER);
    ADCINC_1_Start(ADCINC_1_HIGHPOWER); /* Turn on ADC power */
    ADCINC_1_GetSamples(0);            /* Sample forever */
   
    while(1) {
     if (ADCINC_1_fIsDataAvailable() != 0) /* If ADC sample is ready... */
     { 
         iResult = ADCINC_1_iGetData() + 2048; /* Get result, convert to unsigned and clear flag */
         ADCINC_1_fClearFlag();
     }
 }
}

   

The general system setup as below:

   

VC1=sys/3

   

VC2=VC1/8

   

VC3=sys/1

   

 Analog Power: SC on/RefH

   

RefMax:Vdd/2+/-BandGap

   

OpAmp bias Low

   

A-buff_power low

   

Switch Mode Pump OFF

   

Trip Voltage LVD4.81V

   

Including is my project codes.

0 Likes
2 Replies