ADCINC problem
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
I want to test a very simple code, insamp (with two PGA and one ADC). When I run the code, it stop in the line:

   

if (ADCINC_1_fIsDataAvailable() != 0);

   

Below is the code, can anyone tell me what wrongs, thankks a lot in advance!

   

#include <m8c.h>        // part specific constants and macros
#include "PSoCAPI.h"    // PSoC API definitions for all User Modules
#include "PSoCGPioInt.h"

   

int  iResult;

   

void main(void)
{
    PGA_1_Start(PGA_1_HIGHPOWER);
    PGA_2_Start(PGA_1_HIGHPOWER);
    ADCINC_1_Start(ADCINC_1_HIGHPOWER); /* Turn on ADC power */
    ADCINC_1_GetSamples(0);            /* Sample forever */
   
    while(1) {
     if (ADCINC_1_fIsDataAvailable() != 0) /* If ADC sample is ready... */
     { 
         iResult = ADCINC_1_iGetData() + 2048; /* Get result, convert to unsigned and clear flag */
         ADCINC_1_fClearFlag();
     }
 }
}

   

The general system setup as below:

   

VC1=sys/3

   

VC2=VC1/8

   

VC3=sys/1

   

 Analog Power: SC on/RefH

   

RefMax:Vdd/2+/-BandGap

   

OpAmp bias Low

   

A-buff_power low

   

Switch Mode Pump OFF

   

Trip Voltage LVD4.81V

   

Including is my project codes.

0 Likes
2 Replies
Anonymous
Not applicable

Hi JimL,

   

 

   

Can you please repost the question in PSoC1 topics of the forum?

   

In this space, PSoC5 topics are discussed.

   

 

   

Regards,

   

dasg

0 Likes
MR_41
Employee
Employee
First like received

JimL,

   

 

   

You  need to enable Global Interrupts for the ADC to work.  Add the code "M8C_EnableGInt;" in main.  See if this fixes the problem.  Also, check out my blog post PSoC1 ADCs - The Five Golden Rules that talks about best practices to get the ADC working without any problem.
 

   

Best Regards,

   

Ganesh

0 Likes