- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Situation:
PSoC5 connected to D8-D15 of a 2.8" TFT color module using it as 8-bit parallel interface. Controller is ili9320. Control lines connected accordingly. The TFT module is coming from the STM-32 Mini development board.
Cymodule: Graphic LCD 8-bit Parallel Interface Macro, customized for 8-bits and 3 ClockCycles Low/High pulse width.
Added the SEGGER emWin files to my project according the Cypress installation procedure.
I have added de register initialization settings to the LCDConf.c file at the InitController function.
No errors after building the project but also nothing on the screeen. I only see the RESET function (Light OFF and ON).
Has anyone experience with this type of TFT display or even better has this thing working.....?
I hope to get some suggestions to look after to get my TFT working because I tried everything what comes up in my mind (!).
Thanks!
Rob
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Post project for forum to look at -
“File” Creator
“Create Workspace Bundle”
Use Firefox or IE, not chrome to post.
Regards, Dana.
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
Seems to be a hard question...
Maybe it has something to do with timing? I found that it makes no difference when I change the clock fequency on the input of the Cy module.
Has anyone experiences with the Grafhic LCD 8-bit parallel interface module with or w/o the emWin files?
Rob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have only one project with Grafhic LCD 8-bit parallel interface module for WG240128_5LP.zip here for WG240128R-TFH
I did not use EmWin library from Segger:
- I read: emWin license frozen
- It seemed to me that this too cumbersome and redundant, especially for PSoC4
- I could not find drivers from segger for my displays but found a lot of ready-made private decisions.
But this is just the problem of my qualifications.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Pavlov,
Thanks for info. When I was looking at your set-up, I realized that it was quite the same as mine. So the problem must be in the hardware. And it was....
Self-willed as I am, I found that it should be possible to control the lcd with an 8-bits interface. But I forgot that this display had an other possibility for 8-bits control, namely by using a 8-bits 74HC573 latch, activated by a adding a resistor. And that was the solution.
Before I could start testing, I had to set the Cy interface back to 16-bits, add a LE line in the design to control the latch and modified the original source to split the 16 bits data to 2 times 8-bits, write the low byte into the latch, latched it and write the high byte. Then clocked it into the LCD controller. The 8-bits data from the PsoC is connected to D10-D17 of the LCD module.
On the attached picture you can see the result. Maybe it’s an idea for Cypress to add an new 8-bit Graphic LCD module using a latch, because these kind of GLCD is also very popular.
B.t.w. I had no problem using the (old..) emWin files in my PSoC5 envirement.
Rob
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
Could you please post updated example project. What is your screen resolution and max update rate?
odissey1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Roberto,
Can you please post the updated project file?
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi odissey1 and majed,
Attached my test project.
I made a new module based on the original Graphic LCD Parallel Interface where I modified the .c file to change the Write function into the one that handles the 8-bit interface with latch.
I added to the project the emWin files including the colorbar test file as well.
Rob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Roberto48,
I just downloaded your test project but GUI.h file not found. Can you upload again ?
Thanks
Alptigin