- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I'm used to msp430 counters with set/reset or toggle settings.
But on proc-ble could this be done using just one tcpmw counter, or is two needed?
Or I should use one timmer-isr? and toggle the pins in software, as a stepper motor rpm is pretty low.
on a PSOC the OV & UN using up/down mode could been routed to flipflops, to create this 90deg signal?
Attached is the picture of counter wise stepping on in1 and in2 (ic is a LB1848MC)
- Labels:
-
BLE

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
You are here in the PRoC furum. A PRoC can only perform what you want using two TCPWM components.
In the PSoC 42xx BLE world there are UDB - based components which you may use for your purpose quite better. There you find flip-flops and look-up-tables that will help you generating the two desired waveforms with the appropriate frequency.
A timer isr would be the easiest solution and will probably work up to 1kHz but might get distorted by the BLE interrupts.
Bob