Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
DiBr_284171
Level 2
Level 2
First question asked 10 replies posted 5 replies posted

Compiling  programs on the PIONEER KIT using sprintf  almost uses all the flash memory even for a simple program as shown below:

   

#include <device.h>
#include <stdio.h>
void main()
{
    char tmpStr[10];
    int n =5;
    Tx_Start();
    sprintf(tmpStr,"%d", n);     /* Create a formatted string */
    Tx_UartPutString(tmpStr);  
}

   

Flash used: 30496 of 32768 bytes (93.1 %).
SRAM used: 2412 of 4096 bytes (58.9 %).

--------------- Build Succeeded: 05/21/2013 17:03:04 ---------------
Programming started for device: 'PSoC 4 CY8C4245AXI-483'.

   

Using sprintf with floats completely over flows the flash.

   

ERROR: .\ARM_GCC_441\Debug\HCSR04.elf section `.data' will not fit in region `rom'
The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.
ERROR: region `rom' overflowed by 1032 bytes

   

Is this a bug in the GCC Compiler or  am I missing something?

   

James

0 Likes
12 Replies
Anonymous
Not applicable

it should have 32k of flash. Strange.

0 Likes
Anonymous
Not applicable

Just tried that, looks like it use upto around 30k of flash. I guess you should raise a case for Cypress support.

0 Likes
Anonymous
Not applicable

Tried something simliar in PSoC3, it is around 1k. for PSoC5 is is around 20k. May be there is something to do with the GCC compiler as both PSoC4 and 5 should be using the GCC.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I had the very same isuue yesterday, sprintf() blew up a PSoC4 project requiring 16k flash more than the chip has got.

   

Afaik for PSoC1 Cypress has built 3 different selectable <stdio.h> libraries supporting different complexity for the printf() function requiring different amount of flash. I cannot tell if the GCC  will allow for this.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

I did some search on the net and it seems that this is an common complain with the GCC compiler, Some wrote there own routine to handle this function

0 Likes
Anonymous
Not applicable

Just went thru the creator KP&S, on page 2 it mentioned the sprintf() with float arguement problem (ID 148013) and mentioned that is a detect on the M0 library. The problem may be related to your's. Cypress mentioned a new tool-chainwould be used the next major released.

0 Likes
Anonymous
Not applicable

 Hey guys have you checked the tiny printf for embedded applications?

   

http://www.sparetimelabs.com/tinyprintf/tinyprintf.php

   

Try this guy. He will take very small amount of flash.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

He seems to state if printing longs even his printf()/sprintf() footprint

   

gets large. I have an application that can be used as  a test bed, will

   

try it out when I get a chance.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

good stuff. tks 🙂

0 Likes
DiBr_284171
Level 2
Level 2
First question asked 10 replies posted 5 replies posted

Thanks for all your comments! The sprintf in the GCC compiler gets worse with floats --- no output!. Ran identical code with PSoC5 using Keil compiler and PSoC4 with GCC.

   

#include <device.h>
#include <stdio.h>
void main()
{
    char tmpStr[10];
    float n =-665.67;
    Tx_Start();
    sprintf(tmpStr,"%.3f", n);     /* Create a formatted string */
    while(1)
    {
    Tx_PutChar(10);
    Tx_PutChar(13);
    Tx_PutString(tmpStr);  
    }
}

PoC5:
Flash used: 25628 of 262144 bytes (9.8 %).
SRAM used: 1620 of 65536 bytes (2.5 %).

Tx Output:
-665.670                                                                       
-665.670                                                                       
-665.670                                                                       
-665.670                                                                       
-665.670                                                                       
-665.670
.
.

PSoC4:
Identical code

Flash used: 31180 of 32768 bytes (95.2 %).
SRAM used: 2404 of 4096 bytes (58.7 %).

Tx Output: None
CPU in Limbo

   

Please POST if you have been able to get output from sprintf with floats. Require validation before I create a case.

   

James

0 Likes
Anonymous
Not applicable

 As in my previous post, they already say that spritf with float would cause problem. please check my the creator KP&S.

0 Likes
DiBr_284171
Level 2
Level 2
First question asked 10 replies posted 5 replies posted

The sprintf is not useful for PSOC4 using the present stdio.h implementation. For integer formatting it takes to much flash and for floats it doesn't work at all.  The itoa is not defined in the GCC compiler because it not a standard ANSI function. Here is one implementation of itoa that you may find useful in a future project.

   

/**
     * C++ version 0.4 char* style "itoa":
     * Written by Lukás Chmela
     * Released under GPLv3.
     * http://www.jb.man.ac.uk/~slowe/cpp/itoa.html
     */
    char* itoa(int value, char* result, int base) {
        // check that the base if valid
        if (base < 2 || base > 36) { *result = '\0'; return result; }
   
        char* ptr = result, *ptr1 = result, tmp_char;
        int tmp_value;
   
        do {
            tmp_value = value;
            value /= base;
            *ptr++ = "zyxwvutsrqponmlkjihgfedcba9876543210123456789abcdefghijklmnopqrstuvwxyz" [35 + (tmp_value - value * base)];
        } while ( value );
   
        // Apply negative sign
        if (tmp_value < 0) *ptr++ = '-';
        *ptr-- = '\0';
        while(ptr1 < ptr) {
            tmp_char = *ptr;
            *ptr--= *ptr1;
            *ptr1++ = tmp_char;
        }
        return result;
    }

   

 

   

Tested the above function  on the rangefinder (HCSR401bundle01)project posted on this this forum. Didn't want to wire the 602 LCD Module to the pioneer board so I just  added the Serial Communication Block  to the project  configured as Tx  and outputted  the distance to a virtual PC port.

0 Likes