Announcements

Equip yourself to optimize PSoc4 MCUs for Evs at the EV Webinar. Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

Anonymous
Not applicable

Hi ,

I have following Cypress day020 example to test for uart to ble bridge by programming both peripheral project to kitProg usb dongle and the central project to Psoc ble module. It works great.

However I have another design using nordic and its application of nus service (uart to ble bridge) as central, so I expect that it can also work with kitProg too.

The result is not, they can not even connect.

A close look showed uart to ble is custom service and use custom uuid for the uart bridge service. I found from the creator ide i can modify cypress uart to ble peripheral uuid to match with nordic nus service custom uuid.

I have not quite started to make this hack yet, but wonder if this is the right way to modify as mentioned to allow different vendors uart to ble can connect and exchange uart data to ble as bridge?

Please advise.

Thanks,

Alex

0 Likes
1 Solution
Anonymous
Not applicable

Yes, this is a perfectly acceptable method. Until/unless the BLE SIG group adds a standard UART over BLE service(s), then you will need to implement a custom service anyways.

Different vendors will change bits here and there, but the overall premise and function will be the same, with only the details of UUID, service, data buffer size, etc. changing.

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Yes, this is a perfectly acceptable method. Until/unless the BLE SIG group adds a standard UART over BLE service(s), then you will need to implement a custom service anyways.

Different vendors will change bits here and there, but the overall premise and function will be the same, with only the details of UUID, service, data buffer size, etc. changing.

0 Likes