Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
atga_4655031
Level 1
Level 1
First like given

my questions is

my BLE device is central and peripheral mode.

1) first case- BLE device is central and my android mobile is peripheral.

so peripheral start advertising packet. so my central device is store the peripheral packet in some array.

then i check in data base is that my mobile device mac address match to database then communicate.otherwise disconnect.

2)second case -how ble device switch from central to peripheral.

please solve my issues.

regards,

Atul

atulg@iotech.biz

0 Likes
1 Solution
Yugandhar
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 5 likes given

Hello,


1. Please refer to the Day010_Observer and Day013_Client_Server projects from the GitHub. In this example projects, initially device scans for the nearby advertising devices continuously and shows the advertising report and scan response data of the advertising devices on the UART terminal (like Tera Term, Hyperterminal).

At the central device, in scan progress result event(CYBLE_EVT_GAPC_SCAN_PROGRESS_RESULT), you can check for the particular Advertising device address and can make a connection( Day013_Client_Server project will give the information on connection between two devices).

2. To configure PSoC4 BLE in both Central and Peripheral GAP role you can refer to the Day012_Central_Peripheral example project from the GitHub. In this project, when the device is acting as central, it can scan and connect to peer device which is advertising. When acting as peripheral it can advertise and other Central can connect to the PSoC4 BLE.

Please let me know if this helps.

Thanks,
P Yugandhar.

View solution in original post

5 Replies
Yugandhar
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 5 likes given

Hello,


1. Please refer to the Day010_Observer and Day013_Client_Server projects from the GitHub. In this example projects, initially device scans for the nearby advertising devices continuously and shows the advertising report and scan response data of the advertising devices on the UART terminal (like Tera Term, Hyperterminal).

At the central device, in scan progress result event(CYBLE_EVT_GAPC_SCAN_PROGRESS_RESULT), you can check for the particular Advertising device address and can make a connection( Day013_Client_Server project will give the information on connection between two devices).

2. To configure PSoC4 BLE in both Central and Peripheral GAP role you can refer to the Day012_Central_Peripheral example project from the GitHub. In this project, when the device is acting as central, it can scan and connect to peer device which is advertising. When acting as peripheral it can advertise and other Central can connect to the PSoC4 BLE.

Please let me know if this helps.

Thanks,
P Yugandhar.

atga_4655031
Level 1
Level 1
First like given

hello sir,

thanks sir givening information.

i have one doubt please clear this.

how the central device is scanning the advertising packet.

in advetisng packet so many information how central is know that device is all ready used before.

0 Likes

Hello,

At the central device, in CYBLE_EVT_GAPC_SCAN_PROGRESS_RESULT event, you can check for the particular Advertising device address and make a connection as shown in below code.

******************************************************

       case CYBLE_EVT_GAPC_SCAN_PROGRESS_RESULT:

                scanReport=  *(CYBLE_GAPC_ADV_REPORT_T*)eventParam;
              
                if(scanReport.peerBdAddr[0] == 0x01 && scanReport.peerBdAddr[1] == 0x02 && scanReport.peerBdAddr[2] == 0x03 && scanReport.peerBdAddr[3] == 0x04 && scanReport.data[4] == 0x05 && scanReport.data[5] == 0x0a)
                {
                    printf("peer address:\r\n");
                   for(i=0;i<CYBLE_GAP_BD_ADDR_SIZE;i++)
                    {
                        peerDeviceAddr.bdAddr=scanReport.peerBdAddr;
                        printf("%2.2x",scanReport.peerBdAddr[CYBLE_GAP_BD_ADDR_SIZE-1-i]);
                    }
                    printf("\r\n");
                    deviceDetected=TRUE;
                    CyBle_GapcStopScan();
                }
            break;

        case CYBLE_EVT_GAPC_SCAN_START_STOP:

                if(CyBle_GetState()==CYBLE_STATE_DISCONNECTED)
                {   
                    printf("Stop scanning:\r\n");
                    if(deviceDetected==TRUE)
                    {
                        apiResult=CyBle_GapcConnectDevice(&peerDeviceAddr);
                        if(apiResult==CYBLE_ERROR_OK)
                        {
                            printf("success\r\n");
                        }
                        else
                        {
                            printf("connection failed:%x\r\n",apiResult);
                        }
                        deviceDetected=FALSE;  
                    }
                }
            break;

******************************************************

Thanks,
P Yugandhar.

0 Likes
atga_4655031
Level 1
Level 1
First like given

hello sir,

without UART it is communication possible between central and peripheral.

0 Likes

Hello,

1. Central device is a device that scans for advertisements from GAP Peripherals and establishes a connection with them. When PSoC4 BLE is configured in GAP Central role then after scan start, CYBLE_EVT_GAPC_SCAN_PROGRESS_RESULT will occurs when it receives any advertisement packet or scan response packet from the peer devices. CYBLE_GAPC_ADV_REPORT_T is returned as the event parameter and this structure CYBLE_GAPC_ADV_REPORT_T will contains the advertisement report of the peripheral devices. This Advertisement report will contains the below data.

*****************************************
/** Advertisement report received by GAP Central */
typedef struct
{
/** Advertisement event type
     - Connectable undirected advertising = 0x00
     - Connectable directed advertising = 0x01
      - Scannable undirected advertising = 0x02
      - Non connectable undirected advertising = 0x03
      - Scan Response = 0x04
     */
CYBLE_GAPC_ADV_EVENT_T  eventType;

/** bd address type of the device advertising.
  - CYBLE_GAP_ADDR_TYPE_PUBLIC
  - CYBLE_GAP_ADDR_TYPE_RANDOM
  - CYBLE_GAP_ADDR_TYPE_PUBLIC_RPA
  - CYBLE_GAP_ADDR_TYPE_RANDOM_RPA
    */
    uint8           peerAddrType;

/** Public Device Address or Random Device Address for
    each device which responded to scanning. */
    uint8*         peerBdAddr;

/** length of the data for each device that responded to scanning */
    uint8           dataLen;     

/** Pointer to advertising or scan response data */
    uint8*          data; 

/** Rssi of the responding device.
     * Range: -85 <= N <= 0
     * Units: dBm */
    int8         rssi;

} CYBLE_GAPC_ADV_REPORT_T;
*****************************************

2. Yes, you can make communication between central and peripheral without UART. In the projects, UART is used for displaying the Advertisement packets information of all the devices, sending the controlled commands etc. Please refer to the projects for more information.

Please let me know if you have any questions.

Thanks,
P Yugandhar.

0 Likes