Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
hesc_1314511
Level 3
Level 3
10 sign-ins First solution authored 10 replies posted

hi,

I am trying the new capsense block in autotuning, now all is automatic to set.

I have a trouble, with old capsense block, of Creator, it was possible to make the various settings, now with the new capsense block, it is not possible to adjust anything. In my application, where I use springs resting on a plexiglass, the new block fails to calibrate. Do you have a solution? can you help me?

thanks for help

Henry

0 Likes
2 Replies
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

Hi Henry,

Do you mean that the same product, using the old capsense version can set the parameters and run well, but use the new version, it will fail?

What is the phenomenon when you say "fails to calibrate"?

What  the capacity value the sensor is?

All the sensor calibrate fail or only one sensor?

 

 

0 Likes
MiNe_85951
Level 7
Level 7
Distributor - TED (Japan)
50 likes received 500 replies posted 50 solutions authored

Hello,

 

What are the CapSense components you are using ?

Which is CapSense[v7.0] or CapSense CSD[v2.0] ?

If you select AUTO(Smart Sense) for both components, the parameters that can be set are limited.

First of all, please tell us the types of components and the tuning method (tuning mode).

 

Regards,

0 Likes