PSoC™ 4 Forum Discussions
Dear community,
Working on a project based on CY8C4046LQI-T452 reached the stage where we need to think on the production automation and more specifically on the chip programming. For my great disappointment, there seems to be no options to do a CLI programming using the cheaper(KitProg3) option. From what I have read, reached to the following conclusion:
-Modus Toolbox CLI is not suitable as the make/build option is not desired
-PSoC Programmer does not support the target and is not going to
-mtb-programmer does not have CLI option
The last option left is using a J-Link.
Would appreciate you suggestions
Kind regards
ST
hello, we develop a project with CY8C 4149 and project go very well, we switch the chip cy8c4149 to cy8c4148 and program cyc84148, it got failure. we understand the cy8c4148 has flash memory of 256kb, our firmware size is 235kb, it should allow to be programmed in cy8c4148. following image is the programmer programming result.
Could you help me out to successfully program in cy8c4148
Thank you
Show LessI tried coneccting CySmart 1.3.0.8 and CY8CKIT-042-BLE-A using default settings.
Then, too many peer devices were listed in master tab.
Could I delete peer devices from list when I push [start scan]?
and is there a way to display only Cypress(Infineon) devices on master tab?
Or Could I serch and sort devices with device name?
best regards
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-4/CySmart-configuration/td-p/741035
Show Lesshi, Im music developer try to create new instrument basic on Eastern instrument ,i start my prototype with Arduino board .
I want to change for Infineon microprocessor ,I need same touchkeys function in this link .
- different dimensions keys board
- Bluetooth MIDI/OSC transmit messages controller
- 156 touch switch
- 26 touch keys with full midi/osc controller function
-OLED display
((My main question is which microprocessor i need to start with .))
Show Less
Hi,
When we compared samples of the CY8C4124AXI-443T produced at different dates and factories, the differences detailed below were detected
In order to understand which of these differences in top marking and lead frames are correct, we need your official statements that we can use.
Reverse Logo colors, different alignment and size
TWNxxxx vs xxxx (There is no any Country Code. PHI or TWN)
Different Lead Frames (X-ray image)
Are there any official statements about these differences?
Show LessHellow World example code, is an output string using cy_scb_uart_putString ().
How do I change to printf?
Although retartget-io was found, it can only be used for PSOC6, POSC4 cannot be used.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-4/CY8CKIT-041S-MAX-%E5%A6%82%E4%BD%95%E4%BD%BF%E7%94%A8printf/td-p/648379
Show LessEver see and ADC input that changes if it's watched?
I have an ADC battery monitor that works as expected, ONLY IF you touch it ONE time after startup with anything, like a scope probe or even tweezers. Unless you do this, it reads a very high, impossible high value, as if the VSS is -3.3V.
I realize there is a pin usage error that might cause this, and even though I will probably change it, I just want to understand why it works this way. The error is that Pin 5.1 is OVT tolerant, but P1.6 is not. Even if P1.6 is left low it acts this way, so perhaps when the device is off, the pin protection is latching.
If there is a software fix for this I would be interested in knowing, just because I despise ghosts in the machine.
Thanks.
int32_t MeasD=0;
int32_t retval=0;
VBAT_ADC_Start();
CyDelay(1);
VBAT_ADC_StartConvert();
VBAT_ADC_IsEndConversion(VBAT_ADC_WAIT_FOR_RESULT);
MeasD=(int32_t) VBAT_ADC_GetResult16(0); // Channel
VBAT_ADC_Stop();
Show Less
Hello, I'm using PSoC Creator with a PSoc 4 M-Series Pioneer Kit. I'm trying to run the Deep-sleep Blink example but I am unable to connect to the target. I don't see any target when I select debug target. Is this kit too old for version 4.4?
Thank you
Show LessHello,
I just want to get started with writing simple code for a custom board with theCY8C4148AZI-S553, I downloaded the modustoolbox and the EclispeIDE for modustoolbox but when you create a project and try to select the MCU there is only the option to select kits and the closest kit is CY8CKIT-041S-MAX which uses CY8C4149AZI MCU. Is there another IDE that I can use or a way to use this one to write code for the MCU directly
Show Less