PSoC™ 4 Forum Discussions
Dear cypress society,
Would you please prepare an application note that explains,
Hot to create our own custom profile and integrate our own ble write callbacks into soft,
Thanks in advance..
Show LessI was attempting to use snprintf to format floats into strings to print over UART and I ran into two issues.
Issue 1: "Use newlib-nano Float Formatting" doesn't work.
With the default settings it works perfectly for integers but attempting to use it with floats doesn't work even with the "Use newlib-nano Float Formatting" set to true it does not print the float.
Example:
Value of pi is: to 2dp
In order to get it to include support for floating point printing I had to follow the instructions from http://www.cypress.com/?id=4&rID=87354 and add -u _printf_float to the command line manually and set "Use newlib-nano Float Formatting" to false.
Issue 2: Using snprintf with floats causes the PSoC 4 to hang unless the heap is increased to at least 256B
If you attempt to use snprintf (or sprintf) with floats the processor will jump to IntDefaultHandler and hang. In PSoC Creator 3.1 the default heap size was decreased to 128B from 256B which likely caused this issue.
I have attached a project that should reproduce these issues.
Show LessHi, I've been trying to download the CySmart PC application but keep getting corrupted executables. The website says that the link was updated today (12/31/2014) and that the file size should be 42 MB. The actual files I have repeatedly downloaded on multiple computers are all around 16 MB and are not executable.
Just a heads up, hopefully it's just a bad build that was uploaded to the server. (Otherwise I have really serious internet issues!) If someone else wants to try and download the program and let me know how it works for them I would really appreciate it.
Thanks!
-Brent
Show LessAnyone know when these will be available? I cant seem to find any information about it.
Hi,
Are there any plans to offer the cypress PSoC BLE chips as surface mount modules like the well known "BR-LE4.0-D2A" with antenna onboard? Alternatively, does anyone know of a vendor that sells such a device?
Thanks!
Show LessCan someone tell what is the different between PSoC4xx7-BLE and CYBL10x6x?