Hello, Sir:
my client is more concerned about the patent aspect when doing the program;
is there any introduction of Cypress's touch technology patent?
If so, can you help me to provide it to me?
Thank you very much!
Show LessI2Cバスに仕様上の予約アドレス(0x05など)が流れてきた時、
EZI2CやI2Cコンポーネントはなにか反応して動作したりしますでしょうか?
無視するだけでしょうか?
ご教示いただきたく、よろしくお願いいたします。
I am using the CYBLE222014-01 in an application where I need to put the entire module to sleep in the lowest possible power mode. When in this mode, there is no BLE activity or MCU activity other than an accelerometer programmed to wake the module up with motion. Then the module will do a rest and start from the beginning.
The purpose of this operation is to store the device on the shelf for several weeks in this ultra sleep mode and then wake up when the device is moved.
The battery is 300mAH. Reading through all of the datasheets for this module, if both the BLESS is in deep sleep mode and the system MCU is in hibernate, the current should only be around 25uA. I am drawing 260uA and cant see why.
The only other two devices on the board are the accelerometer and an eeprom. Both of those combined draw less than 10uA.
I have confirmed by reading the BLE state prior going into system hibernation, it comes back as BLESS_DEEPSLEEP. I know the MCU is going into hibernation because the board will auto reset when it receives the interrupt from the accelerometer. Only hibernation mode will do an auto reset. I have also tried CYBLE_Stop(). It gives the same results.
I have changed the SWD pins to GPIO and that didnt change anything.
I am using a timer, I2C, ADC and PWM modules. I run the stop function for all of those before going to sleep.
The I2C pull ups are 2.2K to 3.3V supply.
Anyone have any ideas as to what is causing the extra current?
Show Less
PSoC4をPSoC Creatorを使用して開発しております。
MISRA対応の必要がある可能性が色々調査しております。
1.PSoC Creatorで使用しているコンパイラを変更することは出来ますか?
現在は、Build Settings→Toolchainで選択出来るのは下記の3つです。
「ARM GCC 5.4-2016-q2-update」、「ARM GCC Generic」、「ARM MDK Generic」
実際にBuild出来るのは「ARM GCC 5.4-2016-q2-update」のみです。
ここにサードパーティのコンパイラなどを追加したいのですが可能でしょうか?
可能なサードパティを教えて頂けないでしょうか?
2.「ARM GCC 5.4-2016-q2-update」を最新バージョンに変更することは問題ありませんか?
例えば、現状の最新版と思われるVer10.3に変更する。
変更する方法の資料などはありますでしょうか?
3.ProjectをEXPORTしてIAR社製のコンパイラを使用できることは下記の投稿よりわかりました。
https://community.infineon.com/t5/PSoC-Creator-Designer/IAR-in-PSOC-Creator/m-p/143301
実際に書かれいている方法でhexファイルを作成し書込んで動作確認をしたところ問題ありませんでした。
そこで2点ほど教えて下さい。
3-1.IARのツールで作成したHEXファイルからCYACDファイルを作成することは可能でしょうか?
3-2.BLE OTA External Momory対応のプロジェクト(2つのプロジェクトから成り立つもの)もEXPORTで出来るのでしょうか?
Show LessHello
I am really struggling to implement a fixed duty (50%), variable frequency pwm output (controlled by a pot). - I am trying to generate a variable (+modulated) clock frequency for an external chip.
The only way I seem to be able top do it is by adjusting both the period and compare (as period/2) simultaneously, which feels a little clunky.
would anyone have any other suggestions how this could easily be done?
Many Thanks
Nick
Any pointers how this might be done would be greatly appreciated.
Show LessHow can I create Two PWM Signals in sync with programmable phase shift.
Hi Cypress Developer Community,
Customer Support directed me here to determine if there is a recommended substitute for CY8C27543-24AXI .
I appreciate you help.
Bridget Marasco
Liner Manufacturing
Show Less
I am using PSoC4 CY8C4247AZI-M485 to measure 8 currents and i also want to measure a thermistor. I can not seem to get PSoC to build this is there another way I can do this?
Show Less
Does CYBLE-022001-00 module passed TUV certification?
IF not, what is the tool and guideline about Bluetooth fixed frequency test?
Can we use MBT for test?
Thanks!
Show LessHello,
I later realized that EXTCLK could not be entered into the PLL.
Eventually, a crystal oscillator will be connected to the ECO.
Regarding the current situation, is it possible to input a rectangular wave of a crystal oscillator with the same amplitude as the power supply voltage of the PSoC 4100S Plus to exco.eco_in on P0.6?
Best regards,
Yocchi
Show LessUser | Count |
---|---|
423 | |
229 | |
94 | |
89 |