PSoC™ 4 Forum Discussions
Hi
I want to make an application to get my notifications from an iphone through psoc 4 ble. I'm subscribing to ANCS service, i get the notifications, and after i want that data to send to windows to a java or c# application. What I don't know how to do or if it's possible: how do I make the connection between psoc and windows to send the data.
Show LessHello everybody,
I have the following problem: I have two glued boxes which have only 2 free GPIOs and where I have no acceess to the other GPIOs. The two boxes should be able to communicate via UART. For Tx( transmit) there is a ready-to-use block which I can put on each GPIO.
For Rx, there is no such a ready-to-use block an I have taken the source code from another forum post.(https://community.infineon.com/t5/PSoC-4/Software-Based-Uart-Receive/m-p/220861)
I can only receive characters if there is no delay in the source code. If I have a CyDelay() in my source code, then the Software Based Uart Receive no longer works.
Is there a solution to this? If you use an SCB UART block, you can only use certain GPIO pins. Can the GPIO pin somehow be forwarded to another GPIO pin? I am testing it on the Piosnieer Kit 042 with a PSoC 4200, but on the box itself is a PSoC 4100.
Best Regards
Michael
Show LessHi,
Working on a wireless capacitance sensor based on the CY8C4248LQI-BL583. All components are rated to 85 degC or more.
The sensor works fine in room temperature but raising the temp makes it fail as early as 51 degC.
Failure temperature depends on which software I run on the sensor board. With the simple "Find Me" example failure occurs at around 70 degC.
I have tried heating various components e.g. oscillators and capacitors. But most indications points towards that it is the MCU that fails.
I understand the the information provided is not enough to pinpoint the root cause of the problem. I'm rather asking for troubleshooting advice.
BR
//olto
Show Less
Hi,
We restart an old project developped with CY8C5568LTI-114 and we want to open the associated project. For the moment, we just want to analyse the firmware. After that, we redesign the product and we change the microcontroller.
The problem is we can't open the project because the old microcontroller is not recognize by the software PSoC Creator 4.4.
Could you help us to open this old project please ?
Best regards,
Thomas
Show LessHy,
how can I set an Interrupt or Reset to wake up the Psoc 4 from deep sleep after aprox 5 minutes?
Hello,
Couple questions about the CYBLE-222014-01 BLE module.
Pretty much same question as in this post but looking for some clarification:
https://community.infineon.com/t5/PSoC-4/CYBLE-222014-01-Bluetooth-5-1/m-p/283316
Question 1. Appears the CYBLE-222014-01 has been updated from Bluetooth version 4.2 to 5.1. Has anything changed in the part, or BLE stack, or was is simply qualified to Bluetooth 5.1?
Question 2. In that post is says "CYBLE-222014-01 module is qualified module for Bluetooth Low Energy (BLE) 5.1 specification which supports all erratas up to 5.1 but it won't have feature update." What is meant by the term erratas, why would it support errors? Maybe a different term was intended here or am I missing something?
Question 3. The data sheet has the part number naming convention on page 36. It says:
Should there be a -02 for BT5.0? Or also a -03 for BT5.1? Don't see these part numbers anywhere with those dash numbers.
CYBLE-222014-02
CYBLE-222014-03
Question 4. I've purchased CYBLE-222014-01 modules in the past, a few years ago. Still working great. If I buy the same part today (If I can find them) will I be getting the same part? Did not see any PCN document and the revision history does not show any changes to the part itself. I also looked at the PSoC® 4: 4200_BLE Family Datasheet for clues but no info there on the move to 5.1.
Just trying to understand.
BTW, the data sheet is filled with links that go to www.cypress.com that are now broken.
Thanks in advance.
Mark
Show Less
Dear Sirs and Madams,
We are thinking of outputting PWM output to multiple IOs.
We ware considering using smart IO, In Modus Toolbox, it seems that you can connect to Smart IO directly from the PWM component as shown below :
For example,
When using the PWM0 line, I understand from the data sheet that P2[4] and P3[0] are dedicated terminals for the PWM0 line.
(1)
I understand that this is only available for one or the other, is that correct?
Or can I use both P2[4] and P3[0]at the same time?
(2)
Also, it seems that you can set "smart IO 0 chip out[4]" and "smart IO 1 chip out[0]" from the display.
Is it correct to understand that just checking these checkboxes will output the PWM0 line to "smart IO 0 chip out[4]" and "smart IO 1 chip out[0]"?
In other words, in this case, can the same signal of PWM0 line be output to four options?
Regards,
Show LessHi,
i'm developing an application on "CY8C4147AZI-S455" [PSoC 4100 S family] and i need to manage 4 different PWM signals at same frequency and same duty cycle on 4 different output pins [the 4 PWM must be active one per time (every 4 msec i need to active one of them)]. For the moment i've designed 4 different PWM hw modules configured at same frequency and same duty cycle but i would like to know if it's possible to use [i've not found a solution for the moment] just one PWM hw module connecting it to the 4 outputs using a de-multiplexer [or something similar] to "send" the pwm signal to the desired output. Many thanks and regards
Show LessDoes anyone know if/when this product is coming back in stock - or if it is in fact discontinued? Thanks in advance!
Show Less