Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 4 Forum Discussions

Anonymous
PSoC™ 4
Hi, I have two questions on my project.    1. how to calculate the absolute value of capacitance according to the raw data? Is there a equation to do ... Show More
Anonymous
PSoC™ 4
I want 2.4 KHz frequency on PWM out pin with 50% duty cycle. I added a PWM component, Clock - 1MHz, period - 416, compare -208         In the main loo... Show More
Anonymous
PSoC™ 4
I'm looking for a universal analog signal conditioner to combine all my  sensor needs in one unit controlled by our CPU.    have anything to recommend... Show More
Anonymous
PSoC™ 4
I'm having some issues with my hardware design, which is using the PSOC4 BLE chip (CY8C4217LQI-BL473 to be exact).    I'm testing my hardware using so... Show More
Anonymous
PSoC™ 4
What's the number of SPI interfaces I can configure on the BLE version?  I don't see an explicit number in any of the obvious places in the datasheet,... Show More
trhec_1326566
PSoC™ 4
I am wondering: it is possible to enable/disable bonding on the fly in the application code? Or would enabling/disabling the Encryption requirement on... Show More
Anonymous
PSoC™ 4
Dear all PSoC fans!    I am currently working in a project where a PSoC 4, powered by a battery pack, collects sensor information and sends it via Zig... Show More
Anonymous
PSoC™ 4
Hi,    I have several programming boards of the CY8CKIT-049-41xx (the programmer and the target board can be broken off). I have used up the CY8CKIT-0... Show More
Anonymous
PSoC™ 4
I found the low power handling on PSoC4BLE difficult so I tried to create a more user friendly function: void sleep_ble(BLESleepT request). It it base... Show More
IoVo_297831
PSoC™ 4
Hi all,    I would like to if there is any way to connect the LFCLK to the TCPWM block in PSoC4 BLE. Is there also any way to connect the clock input ... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy