PSoC™ 4 Forum Discussions
hello, I need to know the maximum distance between a smartphone and a EZ-BLE, with the following Configuration :
EZ-BLE only transmitter
smartphone with Android only receiver
thanks for your help, Forgive that I do not speak English good.
Show LessHello everyone,
I just ordered today my new CY8CKIT-042-BLE Bluetooth® Low Energy (BLE) Pioneer Kit! 🙂 However, after going through the pdfs I still cannot find the vital differences between the two included modules (PSoC 4 BLE and PRoC BLE).
In what kind of applications could one module fit but the other? Maybe this should be clearly described in the kit page.
Thank you,
Dimitris
Show LessHello All;
Hope you all doing good!
I'm planning to buy Mac address for my PSoC 4 BLE IC, because in my application 50 units connected to 1 dongle. At dongle side I want to identify the data,meaning want to know which unit is sending that data!
Where can i buy this Mac address? Is it from IEEE or is it a good idea to buy MAXIM EPROM contains Mac adress?
Please advice, thank you!
Regards
kirangkr
Show LessI'm following the AN97060 but with no sucess. Now build without error both on Bootloader and Bootloadable project, programmed the bootloadable project, using Cysmart APP on IOS can found my device with bootloader service.But when try to OTA, the progress is stuck on 0%. When received the special command on custom profile,
my device enter into Bootloader.
case CMD_UPDATE_FW:
if((CmdBuf[1] == 0x55) && (CmdBuf[2] == 0xAA))
{
CyDelay(500);
CyBle_Shutdown(); /* stop all ongoing activities */
CyBle_ProcessEvents(); /* process all pending events */
CyBle_SetState(CYBLE_STATE_STOPPED);
CySysWdtUnlock();
CySysWdtDisable(WDT_COUNTER_MASK);
CyGlobalIntDisable;
Bootloadable_Load();
}
There is a error when I have two Central start at the same time try to scan and connect to two Peripheral.
#1. Two Central device start scan
#2. When receive CYBLE_EVT_GAPC_SCAN_PROGRESS_RESULT,
if the target mac address arrived then CyBle_GapcStopScan().
#3. After receive CYBLE_EVT_GAPC_SCAN_START_STOP try to connect.
But if there are two Central, I always get state=scanning, then report HCI_STATUS 12.
Any idea?
///////////////////////////////////////
Stop Scanning, waiting for Scanning event
CYBLE_EVT_GAPC_SCAN_START_STOP
state: scanning
CYBLE_EVT_HCI_STATUS 12
Hello,
I would like to know if there is a computer software that can send HCI commands via RS232 (when the module is in Direct Test Mode). Something like the BlueTool utility. I am asking this because I could not find any download link to BlueTool computer software. The idea is to have a GUI application and not send the commands using a terminal.
Thank you.
Show LessCan a BLE central, with custom profile, broadcast its presence. In other words is possible to know the presence of a BLE device configured as central, or I need to switch it from broadcaster to central?
Thanks,
Fabrizio