PSoC™ 4 Forum Discussions
Part to program = CYBLE-022001-00
Using the MiniProg3 programmer and referencing the ppcli app notes.
Example : Programming a Chip
OpenPort MINIProg3/848E4756090B “c:/Program Files/Cypress/Programmer”
HEX_ReadFile "c:\\CYBLE-022001-00.hex" //Does this specify the device being used???????
SetAcquireMode “Power”
Acquire
Calibrate
EraseAll
Program
Verify
VerifyProtect
Protect
CheckSum 0
HEX_ReadChecksum
I have purchased and received the new BLE kit but have not yet dug into the features or tried to run it up.
Just had a quick question that someone who has already worked with it may be able to answer.
Does the module support SPP and are there any sample Android apps for routines available?
ie. I want to pair smart phone with the PSCO BLE device and transfer serial data in either direction.
I currently do this with an external Sena OEM BT module but would like to investigate lowered cost using the BT built into the new device.
Thanks
Show LessHi,Cypress engineers
The Bluetooth® SIG recently announced Bluetooth 5 Spec,Nordic has released their BLE 5.0 chip NRF52840, when CYPRESS BLE 5.0 chip will be released? As far as I know, PSOC 6 is not supported BLE 5.0 is only to support BLE 4.2 standards.I believe that there will be a lot of semiconductor manufacturers to support BLE 5.0 chip next year
Show LessHi,
Im trying to get the TFT touch screen v2.0 to work with my psoc 4 development kit but to no avail. I tried to follow both tutorials 72 and 73 but both didnt work. All i see is a white screen. I hope someone out there could share me a working code or tips to make this work.
Thank you.
Amos
Show LessHello freinds: I am trying to run my first program using PSOC 4 BLE kit. I plugged in CYBC4247LQI-BL483 chip in KitProg. When I try to debug/program it fails with a message "port acquire failed". Could anybody help me. I using window 10 computer.
Some other info:
1) When I start PSOC programmer, I dont see any device appearing in its list, unless I plugin the dongle. Even when I have dongle in I am unable to debug/program.
2) I see KitProg appearing in "safely remove and eject media section". In device manager KitProg appears only in portable devices section. When I ask to update the driver, it shows all the drivers updated.
Thank you to all.
Show LessDear all,
I am using CY8CKIT-049-42xx kit to interface with my DS3231 RTC module via I2C,
I tried to initialize the RTC by the following code but did not works, i am not sure about this I2C communication,
please help me , if any example code or project is avilable?
I2CM_I2CMasterSendStart(I2C_SLAVE_ADDR,I2CM_I2C_WRITE_XFER_MODE);
I2CM_I2CMasterWriteByte(0x00);// 00H register
I2CM_I2CMasterWriteByte(0x00);// sec
I2CM_I2CMasterWriteByte(0x00);// min
I2CM_I2CMasterWriteByte(0x00);// hrs
I2CM_I2CMasterWriteByte(0x01);// day
I2CM_I2CMasterWriteByte(11); // day
I2CM_I2CMasterWriteByte(12);//month
I2CM_I2CMasterWriteByte(16);//year
I2CM_I2CMasterSendStop();
Thanks,
Ashok R
Show LessHello I doing use the BLE and the UART communication in PSOC creator.
But I don't have use the BLE in receiver and to transmit with the uart
I had test the program one the 100 project day's, I'm a starter and I don't understand..
Can you help me
Show Less