PSoC™ 4 Forum Discussions
Hi,
I have tried looking for documentation regarding what does the coloring of clock sources mean in PSoC Top Design.
See the image attached.
The new clock color is white but after compilation it changes to purple. What do these colors signify?
-Best Regards
Show LessIn order to reduce the interference, I try to control the channel mapping.
Once the device is connected, try to execute the following.
But sometime it will failed report HCI 0x28 instant change.
So how to improve this?
case CYBLE_EVT_GAP_DEVICE_CONNECTED:
DBG_PRINTF("CYBLE_EVT_GAP_DEVICE_CONNECTED: %x \r\n", cyBle_connHandle.bdHandle);
//CyBle_GapAddDeviceToWhiteList(&peerAddr[deviceN]);
if(channelMap==0){
uint8 b[]={0xffu,0xffu,0x0u,0x0u,0x10u};
CyBle_GapcSetHostChannelClassification(b);
}else{
uint8 b[]={0x1u,0x0u,0xffu,0xffu,0x10u};
CyBle_GapcSetHostChannelClassification(b);
}
Hello, I have noticed that a new release of BLE Component for PSoC has been documented at http://www.cypress.com/file/334116/download
but I am unable to upgrade my V3.20 component in PSoC.
I am interested in using the Software HCI mode, to create a small test application for radio type approval.
Can you tell me when this version will be released ?
I want to use CyBle_HciSendPacket() function to set the radio in modulated and unmodulated TX mode on a single frequency (Low,Medium,High channel) and in continuous receive modes.
Do you have a list of available HCI commands, an Application note that list the commands, or an existing example program ?
Thanks for your support.
Show LessWe are looking where to get best prices for moderate MoQ (1k-2k pieces per order) to buy Cypress' CYBLE-012011-00? We are now waiting for Mouser to get the stock and they offer best prices we have been able to find on the market (4.29EUR w/o VAT for MOQ=1k on date: 16.12.2016).
Have anyone spotted better prices from any other reseller? We prefer EU reseller/distributer.
Show LessI'm still learning the in's and out's of C programing so this maybe a very obvious question. I have a Timer that calls an ISR. In my ISR I have this code:
clockCounter++;
if (clockCounter == 1600) {
Increment_Quadrant_LED_OFF_Timer();
Increment_Quadrant_Reset_Timer();
Increment_Power_Off_Timer();
clockCounter = 0;
}
So that every second it calls those three methods to increment some other timer counters. My though process is that this is the cleanest way to handle keeping track of the timers in the appropriate other classes.
Here is what my Increment_Quadrant_LED_OFF_Timer()
function looks like:
void Increment_Quadrant_LED_OFF_Timer()
{
if (!quadrant_LED_OFF_timer_ENABLED) {
return;
}
quadrant_LED_OFF_timer_counter++;
if (quadrant_LED_OFF_timer_counter >= (QUADRANT_LED_OFF_TIMER_DURATION / DEBUG_DIVIDER)) {
Quadrant_LED_OFF_Timer_Did_Expire();
}
}
Where quadrant_LED_OFF_timer_ENABLED
variable and Quadrant_LED_OFF_Timer_Did_Expire()
are defined in a class call app_Timers
. So this works fine the first time that quadrant_LED_OFF_timer_ENABLED
is set to 1 from my main.c
.
Here is what my Quadrant_LED_OFF_Timer_Did_Expire()
method looks like:
void Quadrant_LED_OFF_Timer_Did_Expire()
{
UART_UartPutString("Quadrant_LED_OFF_Timer_Did_Expire \n\r ");
quadrant_LED_OFF_timer_ENABLED = 0;
quadrant_LED_OFF_timer_counter = 0;
}
So you can see that I set my quadrant_LED_OFF_timer_ENABLED
to 0 here.
If I debug and check quadrant_LED_OFF_timer_ENABLED
after it has been set it's correct at 0. However, continuing in debug if I check quadrant_LED_OFF_timer_ENABLED
in this function Increment_Quadrant_LED_OFF_Timer()
it's set back to 1.
So just to clarify:
void Increment_Quadrant_LED_OFF_Timer()
void Quadrant_LED_OFF_Timer_Did_Expire()
int quadrant_LED_OFF_timer_ENABLED
int quadrant_LED_OFF_timer_counter
Are all declared and defined in app_Timers.c
and Increment_Quadrant_LED_OFF_Timer()
is being called from Cook_Timer_ISR.c
My questions are:
- What my take away from the debugging and my other programming experience is that the ISR is calling
Increment_Quadrant_LED_OFF_Timer()
from a different thread? Which is guess it's not technically a different "thread" but some other location in memory? However if this was the case I'm not sure how I'm getting proper UART output. - Is calling external methods like this to increment other counters the proper way to do this from an ISR? Or should I have a separate ISR for each timer that I need? It seems logical to have one counter that counts every 1 second then just piggy back off that one. Maybe not.
Thanks for any help!
Show LessI have an application needs to measure the pulse width. I used the demo code PWMexample as a start. I added a TCPWM counter component to try to measure the pulse width of the PWM signal. Hope that the counter will start at the rising edge and capture at the falling edge so by reading the capture register I can get the pulse width. But the problem here is: whenever I added start or reload input to the component, the capture won't trigger the interrupt.
Does anyone knows what I missed?
Show LessHello Community,
i´m trying to use the "BLE stack" that is provided with PSoC Creator as static library in a FreeRTOS Task.
My first idea was to call "CyBle_ProcessEvents()" in the Idle Task, but this trail was not successful.
Now, i have created a FreeRTOS Task for the processing of the BLE stack api´s, but this isn´t working as expected too.
The task that processes the BLE stack api´s is at highest priority and it is the only task at this priority.
Also the BLE_bless_isr is at the highest priority.
The problem occurs in the call "CyBle_ProcessEvents()".
Du you have any ideas what i do wrong or why it isn´t possible to call the api´s of the BLE stack static libraries within a FreeRTOS Task?
Because the BLE library is static, i can´t debug it with the debugger.
I have attached the files for the FreeRTOS Task.
Thanks in advance
Show LessHello friends,
I'm novice in BLE area, so excuse me if I ask some stupid things.
What is the maximum baudrate, that can be acvheived with CYBLE-014008-00 module? Is 480kbit/s is possible?
Or, mayby somebody is able to suggest another solution - I need BT/BLE module, which is able to get analog signal, 12 bits at least, with 30kHz samplerate, and to steam it continuously to PC/Smartpone with as low as possible power consumption.
Thank you
Show LessHi,
I have a proximity sensor which consists of a PCB trace of around 15cm diameter. There is a crosshatch shield electrode on the bottom layer of the board, and I want to use this shield electrode to give directionality to the sensor as described in the application notes.
Without the shield electrode connected, I get a proximity sensing distance (SNR>5) of around 140mm. When I connect the shield electrode this drops to around 80mm, and there is very little effect on the directionality of the proximity sensing.
Has anyone else tried to produce a directional proximity sensor using a shield electrode?
I have attached a trace of the Sense and Shield signals. The signals are in phase, but the pulse widths are not stable, is this normal?
Device: CY8C4248LQI-BL583
Regards,
Andy
Show Less