Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 4 Forum Discussions

MiNe_85951
PSoC™ 4
Dear Sirs and Madams,   We have a question about HAL of I2 of PSoC4S MAX.   We are using PSoC4S MAX IMO at 48MHz. Therefore, the I2S clock is set as f... Show More
Miku39
PSoC™ 4
When I try to export a PSoC creator bootloader project to keil MDK, it comes with the warning which says "TOOLS.INI Section'[C51]': missing 'PATH' ent... Show More
yangyong
PSoC™ 4
When I2C slave read and write buffers operation ,the index is incremented。 I can't find a function to reset the array index in the CAT2 Peripheral Dri... Show More
yangyong
PSoC™ 4
In PSoC Creator, I can use the function CapSense_ GetCentroidPos get the slider position.  but, in modustoolbox, I found no function that can get  the... Show More
Anonymous
PSoC™ 4
I've found a community item that there is a linux driver available for the CY8CTMA568.Is this the same device? Where can I get the driver? Show More
yangyong
PSoC™ 4
   I am learning CAPSENSE slide on the CY8CKIT-149.  the routine and my owm project work normally in PSoC Creator IDE.  In modustoolbox2.4 IDE, The  C... Show More
brxic_4278271
PSoC™ 4
  Can anyone here help me validate if "616452" is the Lot Code? What is "575"? Show More
DWOBSER73
PSoC™ 4
Specifically, every time I start a new Debug session, I need to redo the following:Display Watch 1 (Debug->Windows->Watch->1)Display Watch 2 (Debug->W... Show More
Lin_Qiang
PSoC™ 4
当我使用CY8C4146LQS-S423芯片的AD采集功能时,遇到一些问题。当电压值在6V时,采集到AD值大约是6.6V (0x0349),偏差会很大。并且外部供电越小,采集到的AD值偏差越大。 最开始我使用的配置如下: 因为被建议使用内部Verf提高AD采集精度,所以我尝试修改VDDA/2为In... Show More
eremirmak
PSoC™ 4
 We will use  CY8C4247AZA-M483  PArt Number , There will be a lot of cyber-security codes and FUSA algorithms in the products to be designed, I reques... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy