PSoC4をPSoC Creatorを使用して開発しております。
MISRA対応の必要がある可能性が色々調査しております。
1.PSoC Creatorで使用しているコンパイラを変更することは出来ますか?
現在は、Build Settings→Toolchainで選択出来るのは下記の3つです。
「ARM GCC 5.4-2016-q2-update」、「ARM GCC Generic」、「ARM MDK Generic」
実際にBuild出来るのは「ARM GCC 5.4-2016-q2-update」のみです。
ここにサードパーティのコンパイラなどを追加したいのですが可能でしょうか?
可能なサードパティを教えて頂けないでしょうか?
2.「ARM GCC 5.4-2016-q2-update」を最新バージョンに変更することは問題ありませんか?
例えば、現状の最新版と思われるVer10.3に変更する。
変更する方法の資料などはありますでしょうか?
3.ProjectをEXPORTしてIAR社製のコンパイラを使用できることは下記の投稿よりわかりました。
https://community.infineon.com/t5/PSoC-Creator-Designer/IAR-in-PSOC-Creator/m-p/143301
実際に書かれいている方法でhexファイルを作成し書込んで動作確認をしたところ問題ありませんでした。
そこで2点ほど教えて下さい。
3-1.IARのツールで作成したHEXファイルからCYACDファイルを作成することは可能でしょうか?
3-2.BLE OTA External Momory対応のプロジェクト(2つのプロジェクトから成り立つもの)もEXPORTで出来るのでしょうか?
Show LessHi everyone,
I have multiple I2C slaves on a network (they are all psoc4 mcu) and I would like to make a general call from the master to all the slaves using the general call address (0x00). Is it possible to accept general call address using EzI2C slave blocks? I tried finding a way to do it, but could not find any info.
Show LessHi everyone,
so I saw the using the EZI2C Slave (SCB mode) [v4.0], it is possible to have a secondary slave address. I was wondering if it was possible to have the same "secondary salve address" when using a regular I2C (SCB mode) [v4.0] block. I looked for information, but could not find what I wanted.
Show LessI need to send 256 bytes, with a 4 bytes header, for a total of 260 bytes via SPI master.
Everything works fine with TX/RX buffers set to 16bytes, and a 16 bytes data buffer.
No matter what I do, when I increase the size of the data buffer, or the TX/RX buffers, or both, if stalls on the receive buffer full, I cannot find an example with a buffer larger than 8 or data buffer larger than 8, can someone help me understand what I am missing?
I know it is interrupt related, but I cannot figure out what to handle to make this work?
H
Show LessHello, Sir:
my client is more concerned about the patent aspect when doing the program;
is there any introduction of Cypress's touch technology patent?
If so, can you help me to provide it to me?
Thank you very much!
Show LessI2Cバスに仕様上の予約アドレス(0x05など)が流れてきた時、
EZI2CやI2Cコンポーネントはなにか反応して動作したりしますでしょうか?
無視するだけでしょうか?
ご教示いただきたく、よろしくお願いいたします。
I am using the CYBLE222014-01 in an application where I need to put the entire module to sleep in the lowest possible power mode. When in this mode, there is no BLE activity or MCU activity other than an accelerometer programmed to wake the module up with motion. Then the module will do a rest and start from the beginning.
The purpose of this operation is to store the device on the shelf for several weeks in this ultra sleep mode and then wake up when the device is moved.
The battery is 300mAH. Reading through all of the datasheets for this module, if both the BLESS is in deep sleep mode and the system MCU is in hibernate, the current should only be around 25uA. I am drawing 260uA and cant see why.
The only other two devices on the board are the accelerometer and an eeprom. Both of those combined draw less than 10uA.
I have confirmed by reading the BLE state prior going into system hibernation, it comes back as BLESS_DEEPSLEEP. I know the MCU is going into hibernation because the board will auto reset when it receives the interrupt from the accelerometer. Only hibernation mode will do an auto reset. I have also tried CYBLE_Stop(). It gives the same results.
I have changed the SWD pins to GPIO and that didnt change anything.
I am using a timer, I2C, ADC and PWM modules. I run the stop function for all of those before going to sleep.
The I2C pull ups are 2.2K to 3.3V supply.
Anyone have any ideas as to what is causing the extra current?
Show Less
Hello
I am really struggling to implement a fixed duty (50%), variable frequency pwm output (controlled by a pot). - I am trying to generate a variable (+modulated) clock frequency for an external chip.
The only way I seem to be able top do it is by adjusting both the period and compare (as period/2) simultaneously, which feels a little clunky.
would anyone have any other suggestions how this could easily be done?
Many Thanks
Nick
Any pointers how this might be done would be greatly appreciated.
Show LessHow can I create Two PWM Signals in sync with programmable phase shift.
Hi Cypress Developer Community,
Customer Support directed me here to determine if there is a recommended substitute for CY8C27543-24AXI .
I appreciate you help.
Bridget Marasco
Liner Manufacturing
Show LessUser | Count |
---|---|
423 | |
229 | |
94 | |
89 |