Hello,
the code for the temperature sensor DS18B20 works fine using only the display. But when I add the BLE code, I can't get it to work, it disconnects before receiving the temperature value. I have tested the same BLE code with another max30102 sensor and it works perfectly.
Can you help me?
Thank you
Show LessWhen the project has 4 buttons,There is no Rsv pin;but 5 buttons,there is;
The project contains 5buttons,How does this Rsv pin connect in PCB ?
Thanks
Magsense 当使用4个buttons的时候没有RSV pin脚,我现在用5个buttons,这个RSV 在PCB 上怎么接呢?
Show Less
My company recently purchased a CY8CKIT-042-BLE Bluetooth® Low Energy (BLE) Pioneer Kit and CY8CKIT-022 CapSense® Liquid Level Sensing Shield in the hope of using them together. We downloaded the PSOC creator and the PSOC programmer and updated the CY8CKIT-042-BLE KitProg firmware.
We then downloaded the Liquid Level Sensing code example from www.cypress.com/CY8CKIT-022. However on attempting to program the device (LLS_CSD_12RX-042.hex) it reported the hex device didn't match the device we wished to program so it couldn't program it.
There are a number of possibilities, I guess.
I have a CY8CKIT-042, which I can test tomorrow, however I would prefer to use the CY8CKIT-042-BLE kit.
Show LessI may really want to port my PSoC Maker 4.4 activities to ModusToolbox, but it doesn't support the PSoC 4200 family due to the PSoC 4 UDBs, which may be obvious. The PSoC Maker really shows how old it can be and hasn't been updated since October 2020. cps test
Is ModusToolbox expected to fully support the PSoC 4200, and if so, when can we finally expect it?
Show LessHi all,
I'm attempting to enable Miniprog programmer tool Port ID argument handling in my .cli file that I've created. And I will call this .cli using ppcli.exe --runfile.
Example of the my .cli content:
OpenPort MiniProg3/<dynamic port ID here> "C:/Program Files (x86)/Cypress/Programmer/"
As I'm new to PPCLI tool, anyone can advise on this?
Show LessHello everyone,
I have a question. Why is there a string of code at the bottom of the chip? How can this happen? Who knows and tells me why???
Look forward to your reply.
Your soon feedback would be appreciated.
Thank you very much.
Best regards,
Qunt Chen
Dear Sirs and Madams,
We are considering Host Sourced Serial Programming (HSSP) for PSoC4.
Is it possible to provide us with information about the "TEST_MODE" register (0x40030014)?
I've checked the architecture TRM and the register TRM, but there isn't just a detailed description of this register name (address number).
PSoC4 Architecture TRM URL
Register TRM does not mention anything about this register.
PSoC4 Register TRM
Please let us know if there is any reason not to mention this register.
Regards,
Show LessI need some help on best way to sync up multiple (eight) processors talking to each other. I would like to basically make a ring of data, so when I send out the data packet of say 64 bits the intended processor would grabs its section. I am trying to get data to 8 different processors almost at the same time (or as close as possible). Is something that can be done using a USART possibly. Does any one have some experience with this kind of thing and how it can be done effective and fast?
Show LessHi,
I need a USB HID (not CDC !!) bootloader firmware for Psoc4. Does anybody know if such a firmware already exists in cypress universum ?
CDC always needs driver to install. Often user do not like to install driver, so the HID profile is the best solution.
Show LessHi community,
In our designing team, we are using the touch controller CYAT81658-64AS48 in our design and are missing some information in order to proceed in our developments and tests. Would it be possible to share with us the "Programmers Reference Guide" and/or the "Full datasheet with I2C register and programming information"?
Thank you in advance for the support,
Best regards, Dario Maione
Show LessUser | Count |
---|---|
423 | |
228 | |
94 | |
89 |