PSoC™ 4 Forum Discussions
I cannot find any example and kits in PSoc Creator Program. It's show Refresh, but i'm already refresh nothing appear on the screen
PS. the board is already connected with USB and power supply on my PC
Show LessI found some that are made for the arduino, would that work on the pioneer dev kit?
We are looking to build a small diy cnc setup here at the shop and we are more familar with psoc than arduino. So we would like to use psoc for this setup if possible.
Show LessWhy does PSoC creator UI limit the max advertising, scanning intervals and scan window to 10.24 seconds?
Is this enforced in the BLE code?
Thanks
Andy
Show LessI have a project for a CYBLE-022001-00 on a custom board.(attached)
It has WDT and a button interrrupt
Both work fine when low power mode is disabled
When it is enabled ( function EnterLowPowerMode is called in main.c) the counters main_loop_count and _isr_count never increment.
The EnterLowPowerMode function was copied from e.pratt's post for the similar issue so I have no doubts that it works
Any ideas ?
Thanks
Andy
Show LessHi everyone,
I am using Timer interrupt in capture mode.
I want to go to the interrupt every hundred milliseconds
How to set timer settings ?
Is there document about this subject?
Show Less
I am using CY8CKIT-042-BLE and recently came accreoss problem with CY5670 BLE dongle. I am using Windows 8.1 and when CY5670 is plugged into the USB port of the PC its not getting detected. No error message popped by PC.
Before it was getting connected to the PC. I am using PSoC creator 4.1.
Please help to troubleshoot the problem.
Show LessHi, We have a PSoC 4 BLE project, and need to do a customer application on the Android and iOS platform for the OTA function, so i have downloaded the source code of Cysmart appliation, and found there is a OTA folder which stored some source codes of the OTA program, but i can not find any application note related to the coding, how come i can understand the usage of the coding in the OTA folder, even the OTA working flow. Do anyone have any work flow or guideline for the source code usage?
I have downloaded the both the user guide of the Cysmart application as below, but it is just introduction for the Cysmart application, and not useful at all.
http://www.cypress.com/file/198621/download
http://www.cypress.com/file/198616/download
Show LessHi,
Can somebody tell me if and how it is possible to get the CY8KIT-042 BLE kit acting as a Bluetooth tethering device? I would like to connect an Android device via Bluetooth to the kit and let the kit send all the data to an IP network. Sending data to and receiving data from the IP network is not an issue, but getting data out of the Android device is.
I have studied and tried the BLE_IPSP Node and BLE_IPSP_Router examples with PSocCreator 4.1, but the IPSP does not seem to be the right profile for this. When running the IPSP Router example on the kit, the Android device does not see the Bluetooth device. When running the Node example, it is visible for the Android device and it can connect to it, but no data is send from Android to Bluetooth.
So i wonder if i am looking in the right direction or not. It would be great if somebody could give me some directions.
Regards,
Johan
Show LessHi,
When I am trying to work on "Watchdog_PSoC4_Example01", I am getting an error
"WDT Interrupt genereated by PSoC creator will be overwritten by the 'WdtIsr' ISR handler of the GlobalSignal component.........."
This is giving error only for CY8CKIT-044 (CY8C4247AZI-M485), but not for other parts.
Can some one help how to recify it??
Screenshot is attached for reference...PFA.
Show Lessi am considering the CY8C4246AZI-L445 in TQFP48 for a design , we want to program this device using a miniprog 3 and the 5-pin connector , unfortunatly the data sheet and cypress technical support SUCKS and so we are unclear on how to wire this up !
on the 5pin connector we are using:
Pin 2 GND, Pin 3 XRES, Pin 4 SCK and Pin 5 SDIO
The pins are wired to the following pins on the MCU :
PIN36: XRES
PIN16 : SCK
PIN14: SDIO
Is this correct ?
Show Less