PSoC™ 4 Forum Discussions
I have the CY8CKIT-042-BLE kit and I'm trying to test a UART connection with the usb dongle (CYBL10162-56LQXI). I am using the example project SCB_UartComm and testing it with Termite. The Com port and baud rate etc is correct but nothing is being sent or received over the serial connection. Does the example project work with the dongle or is it only for the PSoC?
Thanks for your help I'm pretty stuck.
Show LessHi,
Connect the Remote Control with Windows10 PC,not use Ble Dongle,Remote Control can work.But connect the Remote Control with Ble Dongle,not use Windows 's BLE,and with the trackpad surface and touch others key ,the PC no response,I have already update dongle's software.(PROC BLE and PSoC5LP),I find already connect Remote Control with BLE Dongle,but PSOC5 not work.
Show LessI'm currently doing the fixed stack OTA update code example. I followed all of the steps in the datasheet, but when I try and select the project firmware image, there's no firmware image to be selected in the file explorer. I'm looking in the folder that the firmware image is usually in. What's the problem here?
Show LessHello, I am experimenting with the recently bought CY8CKIT-037 MC evaluation kit connected to the provided BLDC motor in 1 shunt FOC configuration.
I am buffled how to proceed with the PID tuning of the Id, Iq current loops, as I do not understand how I can monitor the Id, Iq current response on Bridge Control Panel: is there any document explaining the process?
Thank you.
Show LessI am able to program the CY8C4013SXI-400 from PSoC Creator via miniprog3. However, my firmware does not seem to run. It's just a simple blinking LED, which works on my other PSoC 5. What could be the problem?
Show LessHello,
I have some experiences on the 4100 Familly (CY8C4125LQI-483)- Now I need a fifth PWM only available on the 4100s family.
My main issue at the moment is the big difference in the watchdog API between both architecture:
I can setup the WDT delay to my needs i.e: 1.6 secs.
I used to "kick" the watchdog using the CySysWdtResetCounters(CY_SYS_WDT_COUNTER0_RESET); to reset the counter on the 4100,
This function is not present on the 4100s. What can I do to reset the watchdog counter on the 4100s device?
Thanks in advance for your reply.
You will find my setting for the WDT settings in the cydrw in the joined picture.
Show LessI've bought the PSOC 4 BLE device development kit. I want to take the small BLE device out from the base. Is it possible? If so, what are the voltage that supply enough power to run the small BLE device?
Thank you!
Show LessHI,
I'm using the Module CYBLE-222014-01.
Calling the function CyBle_GattsNotification() with small packets and a frequency > 9 Hz causes a hanging application (no interrupts any more).
I'm checking busyStatus in advance ( if(busyStatus == CYBLE_STACK_STATE_FREE) .....)
Any ideas for a solution or bug-fix?
Thanks.
Show LessHi,
I am developing a cnc controller using a CY8CKIT-049-41xx kit. For this I need to generate specific number of pulses of set pulse width (equal pulse widths no PWM), pulses for both X and Y axis is required.
The first approach I used consists of pulsing an output high and low, however I also want the kit to send back UART data to a PC. There must be no delays as this can affect the pulse motion.
Is this possible to do this using PWM or the Counter components, ?
My scheme is to do this...
I set the pulse widths, count values, then start the pulsing, since the main program loop is not involved in the actual pulsing I can send data to a PC via UART using the UART component
thanks
a
Show Less