PSoC™ 4 Forum Discussions
Hello
perhaps this has been asked before: is on the roadmap support of Bluetooth Mesh stack for PSoC BLE with Creator in future?
I know this is now supported in the Wiced platform for two Bluetooth MCU, I am just curious if this is going to be added to the PSoC at some point.
Fausto
Show LessHello everyone,
First of all this my first time playing with PSoC creator or with any Cypress PSoC device. And i am really amazed: it's incredible.
Since I have some free time these days I decided to learn about the way that this uC are programmed. So...
I am blinking some leds. I saw that it's possible to access pins as a port which is quite nice. But is it possible to access them from an array?
Below my code. Thank you in advance.
/* ========================================
*
* Copyright YOUR COMPANY, THE YEAR
* All Rights Reserved
* UNPUBLISHED, LICENSED SOFTWARE.
*
* CONFIDENTIAL AND PROPRIETARY INFORMATION
* WHICH IS THE PROPERTY OF your company.
*
* ========================================
*/
#include "project.h"
#include "cypins.h"
int array[4]={LED_1_0,LED_1_1,LED_1_2,LED_1_3};
int main(void)
{
CyGlobalIntEnable; /* Enable global interrupts. */
/* Place your initialization/startup code here (e.g. MyInst_Start()) */
for(;;)
{
for(int i=1;i<16;i++){
LED_1_Write(i);
CyDelay(1000);
}
for(int i=1;i<4;i++){
CyPins_SetPin(??);
CyDelay(1000);
}
/* Place your application code here. */
}
}
/* [] END OF FILE */
Show LessUsing CYBLE-212019 and starting from the 'BLE Hid Keyboard' design example of 'PSoC Creator' I have developed a Bluetooth PC keyboard. Now I have to implement a Bluetooth mouse on the same device.
I've checked the 'BLE Hid Mouse' example and it works and I've tried to merge the two projects copying the mouse service inside the keyboard project and the BLE mouse event management in the code.
Currently it does not work neither the keyboard nor the mouse but may be I've forgotten to copy something.
What I like to know if it's possible to have mouse and keyboard profiles implemented on the same device and, if possible, some info about how to do it.
Many thanks.
Paolo
Show LessIs it possible to put MCU to deepsleep while scanning for BLE advertising packets? I'm able to put MCU to deepsleep during advertising period. But when I do both advertising and scanning, it does not seem to go to deepsleep. I will go to deepsleep after it stops scanning. So, I wonder whether it can be done. Thank you so much in advance. I really appreciate for your help.
Show LessHello.
I am working on a project to remotely reset the CYBLE 022001-00, from Hibernate Mode (based on the pioneer kit -042BLE).
I was wondering whether there are any projects that do this?
The code example in PSOC creator (Hibernate PSoC4 Example) uses a Pin_SW to execute a chip Reset. This will not work for my project, since the objective is to have the Client (iPhone with Cysmart) wake up the peripheral.
Your help will be highly appreciated.
Regards,
Andrew Mugisha
Show LessHi,
I am anxious about the metastable that the gpio input is synchronized with clk by SmartIO.
and I want to input it to TR1 of Data Unit.
Is there no problem?
Or should I synchronize the gpio input twice?
Best regards,
Yocchi
Show LessSelect CapSense's tuning mode as SmartSense(Full Auto-Tune).
Why can not I set the CapSense Modulator clock frequency to less than 6000 kHz?
Which document describes this restriction
CapSenseのtuning modeをSmartSense(Full Auto-Tune)を選択します。
CapSenseのModulator clock frequency を 6000kHzより小さい周波数を設定できないがなぜか。
どのドキュメントでこの制限が記述されているか。
Show LessHi,
I can get some Schematics Symbols and PCB Footprints document,like PSoC_41xxS_Family_Schematics_Symbols_and_PCB_Footprints.zip in http://www.cypress.com/cad-resources/psoc-4-cad-libraries page,but I can find the document of PSoC 4100S Pluse family.Where can I find the Schematics Symbols and PCB Footprints document of PSoC 4100S Pluse?
Show LessMy product uses CYBLE-222014-01 with EZ-Serial V1.1.1 I want to be sure of ordering these parts programmed with the correct firmware. What must I specify to be sure of getting this ?
I have previously asked this question, and been told that all parts after <date> have this, but I have no way of knowing when the parts supplied by my CM were shipped.
Is there a particular first date code or part number I can request ?
The parts I have been given have no recognizable date code and the wrong firmware.
Show Less